Intermittent Pilot Ignition Control, 24Vac, Lockout Timing 90 Sec.

Rollover image to zoom in

Click image to enlarge

Intermittent Pilot Ignition Control, 24Vac, Lockout Timing 90 Sec.

Item #: WBB210957

Sold By: globalindustrial.com

Expected ship date 02/18/2018 Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

{{myData}}

{{myData1}}

{{myData2}}

Price: $ 124.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
When the thermostat calls for heat, the 780-845 control simultaneously initiates ignition sparking and opens the pilot valve portion of the gas valve. Pilot flame recognition stops ignition sparking and opens the main valve portion of the gas valve. Pilot burner flame is continuously monitored at a synchronous frequency for the duration of the heating cycle. Should the pilot flame fail during the heating cycle, the control will shut off the main valve until the pilot flame is established. The 780-845 lockout ignition control provides 90 seconds of spark, followed by a 6 minute time delay (purge) between ignition attempts. After three tries, if no pilot flame is sensed, the control goes into a one-hour lockout period. At the end of the lockout period, if the demand for heat is still present, the unit will repeat the three tries for ignition. Identifying Your Robertshaw ICU Terminals: MV-Main valve, PV-Pilot valve, LED-Dagnostic LED, TH-24V thermostat, PV-MV: Gas valve common, TR-Transformer ground, GND-Main Burner Ground, SENSE-Internal/external sense terminal, SPARK-Spark output. During lockout, you may override the auto-system, and manually reset the unit at the thermostat. The green diagnostic LED will be on continuously for normal operation. The LED will be off for internal lockout and will flash continuously for problems external to the control (ie. not sensing flame).

Product Specifications

    • BRANDRobertshaw
    • LIMITED WARRANTY YEARS1
    • MANUFACTURER'S PART NUMBER100-00834-41

Avg. Customer Rating: (2 customer reviews)

Write your own review

Sort by: 
1 ...

2 Results

Pilot Ignition

Your review: Works Great, quality product! Thanks!

Is this review helpful?

Does as advertised

Your review: When I had to replace my old Pilot ignition module, I was very concerned as my module was no longer produced. This modlule stated it was a direct replacement and even though the connections were in different places, they were all there. I was concerned about the sensor line since the origingal model didn't have one. When I asked how it would work I really didn't get an answer which clarified. I took the discription literally and took a chance and ordered the module. It turns out if you don't have an external sensor line you just plug the wire on module into the connector. Instructions were easy to understand.

Is this review helpful?

Sort by: 
1 ...

2 Results

Be the First to Ask a Question!