Boss Cleaning Equipment Gloss Boss® Mini Scrubber Polisher

Rollover image to zoom in

Click image to enlarge

Boss Cleaning Equipment Gloss Boss® Mini Scrubber Polisher

Item #: WBB286995

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

{{myData}}

{{myData1}}

{{myData2}}

List Price: $109.00 Save up to 25%
Price: $ 82.00

Frequently Purchased Together

Product Information
Photo/Video Gallery
Warranty
Customer Review
Product Q&A
Accessories
Boss Cleaning Equipment Gloss Boss® Mini Scrubber Polisher

The mini Gloss Boss® scrubs, cleans and polishes tile, wood, marble and other hard floors. It removes with ease the most stubborn spots and stains from carpets. Dual counter rotating 470 RPM nylon brushes for deep-down cleaning. Motor turns on by a simple tap of foot pedal and lowering the steel handle. Lightweight (7.6 lbs) and compact design allows cleaning in tight, congested areas. 18 foot cord for operating in large areas without changing outlets. The unit is equipped with two nylon scrub brushes, two microfiber pads for hard floors, two wide-area carpet cleaning bonnets, and two felt pads for wood floors.

Product Specifications

    • HEIGHT INCHES40
    • COLOR FINISHRed
    • BRANDBoss Cleaning Equipment
    • CLEANING WIDTH11
    • CONSTRUCTIONPolyethylene
    • DESCRIPTIONGloss Boss
    • MANUFACTURERS PART NUMBERB200752
    • POWER CORD LENGTH18' Ft.
    • VOLTAGE120
    • WEIGHT LBS7.6
    • RPM470
Have A Question About This Product?
4 Question | 4 | Answer

Avg. Customer Rating: (11 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating

Gloss Boss Mini Scrubber Polisher

This machine works okay, but it is not going to strip your floors like a professional floor buffer would. It will clean your floors, and it will help keep up the job a professional floor buffer would do. *Global Management Comment: This is a floor polisher/shiner, NOT a floor stripper*

See more critical reviews

Sort by: 

11 Results

It's About The Grout Part 2

Your review: After looking a little longer at the portion of the floor tile grout the Boss Scrubber has cleaned in comparison to the untouched dirty grout, I have to be fair and say there is a big improvement and the tile looks much better than it did. So I have to conclude that for the price, this is a good machine. Thank you.

Pros: The Price and size of the machine and ease of use.

Cons: Be nice if the machine had a device to squirt the cleaning product on the grout so us old folks would not have to bend over to apply a cleaning solution to the grout.

Is this review helpful?

I like it ok

Your review: It is not the most sturdy machine, but did a good job on an old concrete floor

Is this review helpful?

Size matters

Your review: IF you are not planning on cleaning a convention center, this is a nice sized machine and cleans well. It doesn't build up your biceps or fy you around the room. I have pets and needed something to scrub tile floors. It did this well although it does take plenty of water to scrub. I have used no other features than the brushes. I would recommend this product for average size homes - 850 sq ft - 2500 sq ft

Pros: Lightweight, easy to store, brushes clean well if enough water is used. Easy assembly. No chemical smells from packaging. Cord wraps nicely on handle.

Cons: little loud, have to make sure you use enough water for brush action to scrub enough

Is this review helpful?

mini scrubber

Your review: Nice little machine

Pros: stores easily - like the turn on feature - unlatch handle, machine turns on

Cons: Must learn to keep even pressure on the brushes. Not a real problem.

Is this review helpful?

Gloss Boss Mini Scrubber

Your review: Serves the purpose I purchased it for. I needed a scrubber to assist in cleaning my basement floor that is covered with a poly coating.

Pros: Light weight. Easy to use.

Is this review helpful?

Boss Mini Scrubber Polisher

Your review: Best product I've bought in a long time. I'm using it to remove the sealer from our marble floor tiles. It saved me a lot of money to do it myself.

Pros: Easy to use. Light weight. Works very well. Priced very good. I recommend this product.

Cons: None so far.............

Is this review helpful?

Gloss Boss Floor Buffer

Your review: This is a pretty good little machine. I was trying to find a replacement for my Hoover floor scrubber / buffer that had a cleaning solution tank and a liquid vacuum. I didn't. But for the price, this machine is just fine.

Pros: Easy to use Extra long power cord Light weight Turns on easily by itself when you press the handle release -- great time saving feature

Cons: It's not as full-featured as my old Hoover floor scrubber It is very light weight. This makes it easy to carry around and store, but not to use -- it should be a bit heavier to prevent skittering across the floor and to hold the brushes in contact with the floor surface.

Is this review helpful?

SOUND

Pros: CLEANSE FLOORS VERY GOOD.

Cons: NEEDS MORE WEIGHT ON THE BUFFING SIDE. CAN CAUSE RINGING IN THE EARS AFTER PROLONG USAGE.

Is this review helpful?

Gloss Boss Mini Scrubber Polisher

Your review: This machine works okay, but it is not going to strip your floors like a professional floor buffer would. It will clean your floors, and it will help keep up the job a professional floor buffer would do. *Global Management Comment: This is a floor polisher/shiner, NOT a floor stripper*

Is this review helpful?

Pullman-Holt Boss Mini Scrubber

Your review: I used it for the first time and I love it. It is lightweight which I need due to shoulder problems and carpel tunnel in both hands. It's very easy to operate and it does a very good job cleaning the kitchen floor.

Is this review helpful?

Lightweight and effective.

Your review: I am using this scrubber on a 500 sq ft area that is covered in synthetic ice. It is a practice area for ice hockey. The flooring requires an industrial size scrubber that is too heavy for me to manage, so I purchased this mini-scrubber. It works very well. It is lightweight and compact . The pads are strong and effective. And the price is affordable. I only wish I purchased it sooner.

Is this review helpful?

Sort by: 

11 Results

There are 11 questions and 4 answers for this product.

Sort by: 

11 Results

We live in an older home with the original hardwood floors that we still wax by hand with Johnson's Paste Wax. We are looking for a buffer to run over the wax to get floors to shine. We have an old polisher that is on it's last leg but want to make sure this will do the job. Thanks!

Question Asked By: Cindy , December 01, 2017

+ View 1 Answer

Answer This Question

Why is it known to the state of California to cause cancer or reproductive harm???

Question Asked By: Michael , San Diego , December 01, 2017

+ View 1 Answer

Answer This Question

Detail item information?

Question Asked By: anonymous

+ View 1 Answer

Answer This Question

I need something to clean my grout of my tile floor. I have a large area to clean and doing it my hand is killing me. Will this work on cleaning grout? are the brushes like scrub brushes?

Question Asked By: Ronda , February 18, 2016

+ View 1 Answer

Answer This Question

Sort by: 

11 Results