Elkay® ezH2O® Next Generation Water Bottle Refilling Stations

Elkay® ezH2O® Next Generation Water Bottle Refilling Stations

Elkay® ezH2O® Next Generation Water Bottle Refilling Stations

Elkay's new line of Next Generations enhanced water bottle refilling stations feature an updated look with a new visual monitor area, for ease of viewing. Water Bottle Refilling Stations can be put into an Energy Savings mode, which can be programmed to power down refrigeration in times of low or non-use.

A diagnostic system is built into the refrigeration system to help get the unit back up and running should there ever be an issue. Filter recognition allows for the unit to recognize the new filter being installed and reset the LED light only by changing out the filter. Low-Energy LED light allows users to easily see when bottles are filled and illuminates dark hallways.


In Stock, Quick Ship Items at Global's Low Prices!

These items are in stock to ship same day and priced low for the best value.

COMPARE
# OF STATIONS REFRIGERATED VR BUBBLER FILTER COLOR PART # IMAGE MODEL QTY PRICE


SAVE BY EMAIL

Exclusive Offers, Weekly Deals!

C&H Government Buyers
Call Us
1.888.978.7759
Chat Online

54.162.10.211:25