Vestil SR-WM, Wall Mounted Storage Rack (1 Pair)

Rollover image to zoom in

Click image to enlarge

Vestil SR-WM, Wall Mounted Storage Rack (1 Pair)

Item #: WB652100

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Qty Price
1-3 $69.95 ea.
4+ $65.95 ea.

Frequently Purchased Together

Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Vestil SR-WM, Wall-Mount Storage Rack (1 Pair)
Store bar stock, lumber and more on this sturdy steel rack equipped with a total of 7 arms: three 18" arms feature a 9" height clearance, and four 15" arms feature a 7-1/4" height clearance for a total rack capacity of 1,000 lbs. of evenly distributed load. Attractive, bright zinc plating. Fast, easy assembly. Measures 60"H overall and weighs 65 lbs. Shown: one pair. Sold in pairs only.

Product Specifications

    • HEIGHT INCHES60
    • CAPACITY LBS1000
    • COLOR FINISHBright Zinc Plate
    • ASSEMBLYUnassembled
    • BRANDVestil
    • CONSTRUCTIONSteel
    • LEVEL QUANTITY7
    • MANUFACTURERS PART NUMBERSR-WM
    • MODEL652100
    • WEIGHT LBS65
    • ACCESSORY DEPTH INCHES15 & 18
Have A Question About This Product?
0 Question | 0 | Answer

Avg. Customer Rating: (9 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

wall mounted storage rack

My company purchased this item to be used for storing our spare railroad crossing gates. Couldn't be happier with the product works as desired looks nice and installation was very easy.

See more favorable reviews

The most critical review

  • Customer Rating

Not worth it

Not impressed with the quality of the product - specifically the little arms that support your stuff - kind of flimsy - if you pull on them some, you can feel that they will give (or bend)

See more critical reviews

Sort by: 
1 ...

9 Results

Not worth it

Your review: Not impressed with the quality of the product - specifically the little arms that support your stuff - kind of flimsy - if you pull on them some, you can feel that they will give (or bend)

Is this review helpful?

Storage Rack

Your review: For the price of this rack you get a whole lot for your money.

Pros: Good solid metal components. Even comes with spare end caps just in case some come off over the life of the rack.

Cons: The assembly instructions are garbage! They have little to no instructions and the pictures are blurry. When assembling you need very nimble hands. Each shelf bracket is secured by a nut and bolt that are almost impossible to put in place with normal sized hands. Be sure to have your metric socket set handy too!

Is this review helpful?

Basic product is good.

Your review: The only issues I have with the product are the instructions and endcaps. The verticals are bookmatched and must be installed with the outside flanges facing each other so that the arms install correctly. Fortunately I realized that before any installation and it was not a problem but the instructions do not call this out clearly. The one real issue I have us the endcaps. They do not come remotely close to fitting and crack upon installation. The ones that I do have installed are cracked and will eventually fall off as they are made of hard plastic. The only possibility for successful installation is to heat them prior to pressing them on and hope they don't crack on cooling. It would be great if Global could provide us with a soft rubber end cap as these are sharp and may be at eye level for some of us. Overall, the product is functional and sturdy and is doing exactly what I needed it to do. I would buy another set in the future if my needs required it.

Is this review helpful?

wall mounted storage rack

Your review: My company purchased this item to be used for storing our spare railroad crossing gates. Couldn't be happier with the product works as desired looks nice and installation was very easy.

Is this review helpful?

Almost an "attaboy"

Your review: Product was what I expected. Assembly was way too complicated / time consuming. Assembly took three time the time it took to fasten to a concrete wall. Assembly hardware count was short in both packages and plastic end caps split upon installation.

Is this review helpful?

Good for the price

Your review: Good product for the price. Not the best, but again for the price it is a pretty good peice

Is this review helpful?

MISSING ITEMS

Your review: The racks are great. But 8 of the gold cap ends were missing so it looks funky.

Is this review helpful?

Storage Rack

Your review: Rack works well and more than adequate for my needs to store PVC Pipe in the warehouse. Easy install too.

Is this review helpful?

lumber rack

Your review: I purchased this wall mounted rack to organize the lumber in my garage. It was able to handle all of the material I had and was very easy to assemble and install. One thing that you should pay attention to is how the product is packaged for shippment. Mine was vertually destroyed when I received it. Lucky I only was short one yellow end cap.

Is this review helpful?

Sort by: 
1 ...

9 Results

Be the First to Ask a Question!