Gas Limit Controls

Gas Limit Controls

Honeywell Gas Limit Controls Are Used For Use As A Fire Thermostat In The Duct Work Of Air Conditioning And Ventilation Systems.

Opens a line or low voltage circuit if the air temperature reaches a critical level at the controller location. If the circulated air reaches a temperature indicative of fire, the limit control shuts off the fan, preventing the fan from contributing to the spread of fire. Also suitable for use with any warm air furnace to provide positive lockout of the burner in the event of fan failure.


COMPARE MANUFACTURERS
DESCRIPTION SWITCH TYPE ELEMENT INSERTION L" PART # IMAGE MODEL QTY PRICE


SAVE BY EMAIL

Exclusive Offers, Weekly Deals!

C&H Government Buyers
Call Us
1.888.978.7759
Chat Online

54.83.81.52:66