Switching to Eco-Friendly Snow Blowers: Saving Money and the Planet
If you haven’t noticed, there is a growing trend to move away from using just about anything that’s gas-powered. With every new mandate – from the New York legislation that proposes a ban on selling new, internal combustion engine vehicles by 2035 to ending the production of gas-powered lawn equipment by 2024 – we’re moving ever closer to a total reliance on electric tools. So, what’s the problem with that? Frankly, perception. Many people are convinced that battery-powered equipment is somehow inferior to their gas-powered counterparts. But nothing could be further from the truth.
In fact, side-by-side comparisons involving everything from vehicles to landscaping equipment, durability, reliability, and power are very similar. As the proof begins to mount, one piece of equipment to keep top of mind as we approach the winter season is a snow blower. While cordless electric snow blowers have been around for years, they are now poised to sit atop the leaderboard when it comes to making the most intelligent purchase for your snow moving needs. And two of the most dependable models on the market today come from EGO and Snow Joe. (pictures)
More than avoiding cutting the power cord during use, the electric portable snow blowers like the ones we offer at Global Industrial are more convenient. When considering the quick charge and easy to switch batteries it makes working outdoors better for you and the environment. But that’s not where the comparison ends. According to Family Handyman, an authority on tools and equipment, an electric cordless snow blower offers users a solution that’s inexpensive, lightweight and one that requires far less maintenance, creates no fumes and is easy to store. With that in mind, let’s look at a few other reasons to consider an electric snow blower over gas snow blowers this winter season.
REASONS TO CONSIDER AN ELECTRIC SNOW BLOWER
ZERO EMISSIONS:
A snow blower without a combustion engine means no need for gasoline. And no gasoline means no hydrocarbons in the air. Cordless electric snow blowers, on the other hand, create zero emissions. None. Nada. Zip. Period.
MAINTENANCE COSTS:
Beyond the gas, a fuel powered snow blower has an engine that includes air filters and spark plugs that need regular attention to keep the engine running properly. And with an engine, comes the engine parts that need oil. All of this adds up to time and energy you could be putting into removing more snow. And when it comes to snow blower cost, gas models are typically among the most expensive models to purchase. In addition, they require gas and as gas prices remain high, they are proving to not be the most cost-effective choice you can make when it comes to keeping your sidewalks and driveways snow free.
NOISE POLLUTION
Keeping the noise down isn’t just about being easier on the ears, it also comes down to safety. When equipment is quieter it makes communication between employees easier and helps to avoid miscommunication. A quieter snow blower machine also makes hearing other machinery like nearby trucks and forklifts easier. Cordless electric snow blowers make virtually no noise when working and even less when in neutral.
EASY OF START
Instead of fighting the pull cord of a gas-powered heavy duty snow blower, just press a button. Yep, it’s that simple.
A BETTER ROI
Unlike the engine and maintenance of a gas-powered snow blower, cordless electric models require a replacement lithium-ion battery. And as it turns out, the type of batteries used for cordless electric equipment are often designed to be used with more than one type of tool, saving you money in the long run.
Our goal at Global Industrial is to help you prepare for what’s ahead. As winter approaches, keep in mind that we offer a full line of good snow blowers and tools that enable you to improve conditions around your property this season and beyond. Learn more about all the ways we can help you by contacting one of our Global Industrial sales representatives at 888.978.7759 or contacting us here.
The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.