Dryer Booster
See all 9 items in product family

Dryer Booster

Item #: WBB449147

Sold By: globalindustrial.com

Usually ships in 2 to 5 days Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 180.95
Product Information
Customer Review
Product Q&A
No on-site wiring. This Dryer Booster turns on and off when the dryer turns on and off automatically. Adjustable air pressure sensing switch is mounted on fan and pre-wired at factory with 10 foot line cord. Includes probe. Just plug it in.

Product Specifications

    • AMPS1
    • AMPS RANGE0-1
    • BRANDAcme Miami
    • CFM HIGH120
    • COLORSilver
    • CONSTRUCTIONSteel
    • DEPTH INCHES7
    • DESCRIPTIONClothes Dryer Vent Booster
    • DIAMETER INCHES4
    • DUCT SIZE INCHES4
    • FAN DIAMETER INCHES4
    • INCLUDESDryer Booster, Pressure Sensing Switch, Probe for Switch
    • INLET/OUTLET DIAMETER INCHES4
    • LENGTH INCHES17
    • LENGTH RANGE12-24"
    • MANUFACTURER PART NUMBER9460
    • RPM HIGH--
    • VOLTAGE115
    • VOLTAGE RANGE115-120
    • WATTS--
    • WIDTH INCHES6
    • WIDTH RANGE1-12"

Avg. Customer Rating: (5 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Very easy to install

The only issue I had with this unit is that the inlet is higher than the outlet for the dryer which made it so that I had to have a "U" shape in the hose feeding the booster. Not an optimum way to plumb it. Otherwise the unit works as it should as we have an 8' rise, 4 90s and about 25' run to the outside wall. The booster pushes the air out and reduced drying time.

See more favorable reviews

The most critical review

  • Customer Rating
Sort by: 

5 Results

Works

Your review: Works but build quality could be better

Is this review helpful?

Considerable improvement

Your review: Very pleased with the Dryer Booster. It fit behind washer and saved considerable effort in re-ducting. We estimate it has reduced drying time by 30-40%, maybe more on some loads.

Pros: quiet, relatively small footprint, easy to install, reasonably priced

Cons: feet attachment could use improvement (w screws or nut/bolt) as one was stripped and needed to be re-drilled. Also, the vent probe, for flexible vent lines, could use some type of screw on attachment with seal on both sides as probe won't seat in flexible line in appropriate position by itself very well (made my own attachment set up)

Is this review helpful?

Worked as Advertised - Great Product

Your review: The booster solved my problem of condensation building up in the vertical portion of the vent (which in turn was flooding my laundry room as it cooled). The only reason I didn't give it 5 stars is because the screws that hold the three legs in place do not tighten well and thus the two of the three legs kept slipping to one side or the other. I finally got them stable, but that's one design that could be improved. However, since that is NOT critical to the main function, I still give the unit high marks. Works just as advertised. It may also be worth noting that the sensor that detects flow (in order to activate the booster) depends on INCREASED air pressure that is only achieved if the unit is completely attached to both intake and output vents. I initially made the mistake of leaving the output vent unattached and was not attaining the required pressure to activate the blower motor. A call to the manufacturer (on Sunday, I might add) steered me in the right direction.

Pros: Excellent power and very quiet

Cons: Loose and wobbly legs

Is this review helpful?

Dryer Booster

Your review: Easy to install, seems to be working well.

Is this review helpful?

Very easy to install

Your review: The only issue I had with this unit is that the inlet is higher than the outlet for the dryer which made it so that I had to have a "U" shape in the hose feeding the booster. Not an optimum way to plumb it. Otherwise the unit works as it should as we have an 8' rise, 4 90s and about 25' run to the outside wall. The booster pushes the air out and reduced drying time.

Is this review helpful?

Sort by: 

5 Results

There are 5 questions and 1 answers for this product.

Sort by: 

5 Results

can I use this as a final lint trap for an indoor residential dryer?

Question Asked By: Eddie , November 29, 2011

+ View 1 Answer

Answer This Question

Sort by: 

5 Results