Continental Fan LT100 Lint Trap
See all 18 items in product family

Continental Fan LT100 Lint Trap

Item #: WBB177931

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $40.00
Product Information
Warranty
Customer Review
Product Q&A
Lint Trap

May be installed between the dryer and the booster fan to help reduce lint build-up in duct and maintenance to the fan. Improves drying capacity. 26 gauge corrosion resistant, satin coat steel can be painted to match decor. Mounts flush to drywall surface. Ceiling or wall mount option. 9/16" mounting flange. One piece door with intergral screen. Galvanized mesh filter. Sturdy slide mechanism is simple to use. This optional lint trap can be used with Dryer Booster Kits.

Product Specifications

    • BRANDContinental Fan
    • COLORSatin Coat
    • CONSTRUCTIONSteel with Galvanized Mesh Filter
    • DEPTH INCHES6-1/8
    • DESCRIPTIONLint Trap
    • HEIGHT INCHES8-7/8
    • HEIGHT RANGE1-12"
    • INLET/OUTLET DIAMETER INCHES4-1/8 Inlet 3-7/8 Outlet
    • LIMITED WARRANTY YEARS1
    • MANUFACTURER PART NUMBERLT100
    • WIDTH INCHES6-1/8
    • WIDTH RANGE1-12"
Have A Question About This Product?
4 Question | 4 | Answer

Avg. Customer Rating: (10 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating
Sort by: 

10 Results

Lint Trap

Your review: the box does not close properly causing lint and hot air to escape. We have lined the edges with rubber lining and place clips on the lid to keep it closed

Pros: Catches lint

Cons: Does not close lint escapes hot air escapes

Is this review helpful?

Excellent secondary trap

Your review: My application was the vent blowing onto the roof so wanted to have a secondary filter and this provided an excellent solution.

Pros: easy to install, requires small amount of space right behind the dryer

Cons: There is a slight gap under the internal screen since it is designed with a bow. There could be a strip to block.

Is this review helpful?

lint trap

Your review: just what I needed a little pricey with shipping tax etc didn't get a chance to price sears unit

Is this review helpful?

Lint Trap

Your review: Does anyone have any ideas as to how to seal the lid to the base. It would require using some sort of gasket that is heat tolerant as the lint trap does get quite warm depending on the dryeer cycle. I also have tried to use a "clip" to hold the lid tighter to the base.

Pros: I installed the lint trap and it is working as it should. The trap was installed as part of a total replacement of the dryer vent from the wall to the outside. After installing the vent, I ran the dryer without any contents three times. It is amazing the amount of lint that came out of the dryer. My clothes now dry in half the time.

Cons: There are two problems with the lint trap. First, it does not seal all the way around the top. This causes lint "dust" to escape which intern can create a fire danger. There needs to be some sort of gasket around the lid to create a tight seal. Also, there are no attachment points on the outside of the trap. Because of this, you are forced to drill trough the bottom of the trap to attach it to the wall.

Is this review helpful?

Great trap

Pros: My dryer's trap is horrible- within 3 months my dryer wouldn't dry anything because the vent was full of lint. I purchased this lint trap and it catches about the same amount of lint that the dryer's lint catches. This is a great product and easy to install.

Cons: One minor con is that the screen doesn't touch the bottom of the box and allows a very very minor amount of lint to go through. The space is about a centimeter opening.

Is this review helpful?

Lint Trap

Your review: I installed this lint trap in a customers basement area that was unfinished. I had to fabricate a mounting bracket that would hold it to a block wall. Works great. Product photo should be upgraded to current model. It would also be nice to have direction of air flow if it makes any difference.

Is this review helpful?

Gas Dryer Lint Trap

Your review: Product is performing as expected.

Is this review helpful?

Good, simple product

Your review: I recently purchased your external Lint Trap. It was exactly what I expected. It was easy to install and seems to be working great.

Is this review helpful?

Lint Trap

Your review: Item arrived quickly and packaged very well. Will use Global again

Is this review helpful?

lint trap

Your review: Very good value. Installed easily. Very effective for stopping lint that gets past the lint trap that is inside the dryer. Easy to remove and clean the screen. The unit I received is not exactly as pictured in the photo. Mine has no window in the door like the photo seems to show. Also, the screen, which is shown diagonally inside the metal box, separate from the door, is actually welded directly to the inside of the door. This welded design probably makes removing the screen for cleaning much easier.

Is this review helpful?

Sort by: 

10 Results

There are 10 questions and 4 answers for this product.

Sort by: 

10 Results

Does this product have to be installed in an upright position

Question Asked By: Michael , December 26, 2014

+ View 1 Answer

Answer This Question

Someone asked the question but it was not directly answered. Can this be used with a GAS dryer?

Question Asked By: scott , December 26, 2014

+ View 1 Answer

Answer This Question

My question is two-fold. Can this trap be used with a gas dryer? The outlet lines for the dryer vent run in the garage in a protected enclosure on the floor. Can the trap be mounted on the floor with the trap "door" facing up? Thanks in advance for your help.

Question Asked By: Michael , home , February 27, 2013

+ View 1 Answer

Answer This Question

can I use this as a final lint trap for an indoor residential dryer?

Question Asked By: Eddie , November 29, 2011

+ View 1 Answer

Answer This Question

Sort by: 

10 Results

SAVE BY EMAIL

Exclusive Offers, Weekly Deals!

C&H Government Buyers
Call Us
1.888.978.7759
Chat Online

54.205.19.31:23