Flip Up Keyboard & Mouse Tray For Orbit

Rollover image to zoom in

Click image to enlarge

See all 39 items in product family

Flip Up Keyboard & Mouse Tray For Orbit

Item #: WB250966

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $74.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Folding Keyboard/Mouse Platform

Platform arm allows convenient storage of keyboard and mouse and folds up or down when not in use. Easily installs on Global Industrial™ Orbit Columns and Posts (sold separately). Made using durable steel. Pullout knob allows 3-position adjustment for up, flat or down positioning. Keyboard platform is adjustable from 5-1/2D to 9D. Keyboard platform adjustment allow clamps keyboard in place using 2 hand screw knobs. Includes 18W x 3-3/4 padded wristrest for enhanced support. Includes width adjustable mousepad with built-in wristrest. Mousepad measures 8-1/2W x 10-1/4D. Includes a mouse holder for convenient storage. Mounting bracket measures 4-3/4W x 4-1/2H with mounting holes spaced 2-3/4 apart. Bracket allows installation to Orbit posts or can be mounted to wall. Measures 18W x 20D overall.

Product Specifications

    • WIDTH INCHES18
    • DEPTH INCHES20
    • COLOR FINISHBlack
    • BRANDGlobal Industrial
    • LIMITED WARRANTY1 Year
    • TYPEKeyboard Tray
    • DESCRIPTIONFlip Up Keyboard & Mouse Tray
    • CONSTRUCTIONSteel
    • MODEL250966
Have A Question About This Product?
2 Question | 2 | Answer

Avg. Customer Rating: (18 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating
Sort by: 

18 Results

Best Seller

Your review: I was so happy to deal with them.

Is this review helpful?

awesome quality

Your review: I was not expecting this product to be such high quality. I thought it would be made of cheep aluminum and that it would buckle under the weight of the keyboard like all the other wall mounted keyboard stands i have tried. THAT WAS NOT THE CASE HERE.

Pros: heavy duty construction. it will not bounce or sway when using it. As sturdy as using a real desk.

Cons: a bit heavy for old drywall but with a little reinforcement not a big deal.

Is this review helpful?

Solid, not long lasting

Your review: These units were purchased to go in a doctor's office, where we use them daily. They're great for the job in terms of function, but longevity seems to be an issue. We purchased four of them in October of 2012. We had to replace the first one in May of 2016. We had to replace the second one in June of 2016.

Pros: Very durable and strong.

Cons: Though it looks like something made of high-grade steel, the pins that allow it to lock up or down seem to wear out after about three years. This is too expensive to have to keep replacing every three years.

Is this review helpful?

Works great for just a wall mount!

Your review: I have bought 2 of these over a timespan and even though this is for a Orbit, it will also work as a wall mount keyboard.

Pros: Great product for the price. 4 holes for a sturdy installation. Doesn't stick out to far so the flip up/down really wasn't needed but is a good addition.

Cons: None that I ran into.

Is this review helpful?

Compact

Your review: We used it on the end of a pallet rack, its compact when folded to allow forklift to get by without any issues.

Pros: Compact design Sturdy Adjustable allowing for different keyboard sizes

Cons: Could use pegs at the end of the mouse pad slider to prevent from over pulling. a little rubber cap fixes this problem.

Is this review helpful?

Flip up keyboard tray

Your review: This is ideal for a community monitor and keyboard at our facility

Pros: It worked really well for our needs

Cons: It would be nice if it had a way to install the mouse pouch to the assembly as I fabricated one.

Is this review helpful?

Wonderful!

Your review: I was looking for an affordable standing desk solution - trying to be healthier this year - and this worked perfectly for my DIY unit. I mounted this keyboard unity to a book shelf (real wood) mounted to the wall with heavy duty anchors and it works great. Additionally, I mounted my flat screen monitor to the same shelf with a $15 wall mount.

Pros: It flips up and down.

Cons: It is heavy, so you need to mount it with heavy duty bolts and anchors.

Is this review helpful?

Flip up keyboard and mouse trey

Your review: Works great, my team member in that area is very happy!

Pros: Adjustable

Cons: none

Is this review helpful?

Keyboard

Your review: Great service - quick delivery

Pros: Great service - quick delivery

Cons: none

Is this review helpful?

flip up keyboard

Your review: very easy to install. Works well. I am not using the mouse tray, looks nice.

Is this review helpful?

Great Product

Your review: This keyboard is so useful at my workstation. AT times i do not have much room to work with and this flips up right against the wall giving me the space i need when i need it.

Is this review helpful?

Good quality but lacking adjustment

Your review: This is a very sturdy item but it only has an adjustment at 180 degrees (straight down) and 90 degrees. I needed it to be adjustable at more than just straight out and put away. I would have like for it to have at least 1 more adjustment spot at 45 degrees.

Is this review helpful?

Perfect keyboard tray for wall mount monitors

Your review: I have just installed touchscreen wall mounted computers in my office to begin using electronic health records. I needed to mount the keyboard underneath the screen, but have it fold out of the way. This tray fit the bill perfectly! Not only is it solid and well constructed, but it is very reasonably priced. It is adjustable to hold almost any size keyboard and grips it securely with 4 high density foam blocks. I don't need the mouse tray, but it works well. It would be a little small if you needed to use it intensively. It is well designed and tucks underneath if not needed. I mounted the tray to the stud in the wall with one set of holes and used toggle bolts through the drywall for the other 2 holes and it is very secure. You can also use Global's rail system to mount both computer monitor and keyboard. I would highly recommend it.

Is this review helpful?

Fit the need,

Your review: Well made; easy to assemble; reasonable price. I wall mounted the unit into a block wall.

Is this review helpful?

Keyboard and Mouse Tray

Your review: Great product! Sturdy and functional! I highly recommend!

Is this review helpful?

Solid

Your review: This tray is extremely well build.

Is this review helpful?

Great product

Your review: What I expecteed in a good product like this.

Is this review helpful?

Great product and great value

Your review: I ordered two of these for standing workstations at our office and we love them! When I looked online these were by far the best priced items, especially since they included the mouse attachment. We anchored them directly into the wall, without the mounting strip. My only recommendation is that you make sure it goes into a stud, since we didn't at first and it came crashing down while working...our fault, though. Now it is anchored more securely and works great!!

Is this review helpful?

Sort by: 

18 Results

There are 18 questions and 2 answers for this product.

Sort by: 

18 Results

Does the keyboard shelf swivel?

Question Asked By: Andy , May 29, 2015

+ View 1 Answer

Answer This Question

When multiple cabinets are ordered do they come keyed alike or keyed differently?

Question Asked By: Alex , Putnam Ct , September 10, 2014

+ View 1 Answer

Answer This Question

Sort by: 

18 Results