Aervoe 800 Vers-A-Striper Line Striper

Rollover image to zoom in

Click image to enlarge

See all 8 items in product family

Aervoe 800 Vers-A-Striper Line Striper

Item #: WB442647

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $84.29 Save up to 12%
Price: $ 73.95

Frequently Purchased Together

Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
VERS-A-STRIPER LINE STRIPER
Aerosol striper is ideal for parking lots, warehouse aisles, school yards, road surfaces, tennis courts, baseball and track fields and more! Portable, lightweight and corrosion resistant line striper is fast and accurate. Just drop the aerosol spray can into place, line up the pointer and squeeze the handle. Gives great looking results every time! Stripe adjusts from 2" to 4". Nose mounted pointer aids in tracking. Includes storage tray that holds up to 12 aerosol cans to allow easy access spray can replacement and disposal.

Product Specifications

    • CAPACITY20 Oz. Aerosol Spray Cans.(12 Spare Cans)
    • COLOR FINISHYellow
    • ASSEMBLYAssembled
    • BRANDAervoe
    • CONSTRUCTIONSteel
    • MODELVerse-A-Striper
    • SIZE2" to 4"
    • TYPEFor Pavement
    • WEIGHT LBS16
Have A Question About This Product?
0 Question | 0 | Answer

Avg. Customer Rating: (28 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

excellent value

Very easy to assemble and use. I'd never used one before and was able to neatly stripe a 40 space parking lot in less than 1 hour. Before you start make sure T-nozzle on spray can is perpendicular to line direction.

See more favorable reviews

The most critical review

  • Customer Rating

Disappointed

Picture of the stripe is incorrect, shows the size to be much larger than it is. Very, Very misleading,will not order anything else after this.

See more critical reviews

Sort by: 
1 2 ...

28 Results

excellent value

Your review: Very easy to assemble and use. I'd never used one before and was able to neatly stripe a 40 space parking lot in less than 1 hour. Before you start make sure T-nozzle on spray can is perpendicular to line direction.

Is this review helpful?

Sprayer

Your review: works perfect

Is this review helpful?

Received/ On Time

Your review: Thank you for this product, it was received on time.

Is this review helpful?

Works as expected.

Your review: It took a few test trys to get a feel for how it sprayed, but after getting the hang of it, it looks like my guy has been striping for years.

Pros: Easy to use, good results.

Cons: None yet.

Is this review helpful?

Excellent tool for the price

Your review: Did a better job than expected.

Pros: Easy to use.

Cons: None

Is this review helpful?

Great product!!

Your review: I bought this product and wasn't sure why the lines were not correct. I contacted the phone number to the company and a person called me back immediately. The product then worked great. I am happy with the product!!

Pros: Price and quality!!

Cons: Time it took to receive it!

Is this review helpful?

Good Quality

Your review: Good quality for the design.

Pros: Good quality

Cons: Wish I could see the ground ahead of the spray to know when to start/stop/turn.

Is this review helpful?

Parking lot line striper

Your review: Easy to assemble (basically attaching handle), easy to use, walks in a straight line. Affordable.

Pros: Ease of use, affordable.

Cons: none

Is this review helpful?

width

Your review: I probably did something wrong, but I couldn't get a parking space line width, only a narrow two inch stripe. I had the can unit raised to the very top.

Is this review helpful?

Inventory Controller

Your review: Easy to set up and use.

Is this review helpful?

Basic model

Your review: I should have gone for better model. Our pavement is getting pitted and I could not get a good crisp line.

Is this review helpful?

Vers-A-Striper Line Striper

Your review: worked exactly as stated. i striped my entire lot of 35 car spots in under 3 hours and saved hundreds of dollars. best price here

Is this review helpful?

Disappointed

Your review: Picture of the stripe is incorrect, shows the size to be much larger than it is. Very, Very misleading,will not order anything else after this.

Is this review helpful?

Line Striper

Your review: It made the job much easier. Thank you.

Is this review helpful?

Exellent product for the money

Your review: This striper is exellent for small jobs such as parking areas or for any small job. It's easy to use.

Is this review helpful?

excelent

Your review: Works great

Is this review helpful?

4 stars

Your review: awesome

Is this review helpful?

Small Parking lot usage

Your review: lightweight, almost portable. Little flimsy on the metal material, but should work for what we need.

Is this review helpful?

Vers-A-Striper

Your review: Easy to use. Quick setup. Had my striping done in half the time of tape and painting.

Is this review helpful?

A real time saver

Your review: We purchased the versa stripper to paint the lines on our church parking lot. We were very impressed by how well our lines came out. We used an 18 foot 2x8 to act as a guide. I definitely would recommend this stripper if you want to save money and time. The price was lower than I have seen it sold at other places.

Is this review helpful?

Did the Job

Your review: Easy to use, only complaint is the wing nuts that hold the handle assembly to the body do not stay tight, I will be replacing them with nylon lock nuts.

Is this review helpful?

vers-a-striper

Your review: Great price, very easy to use and line up. the extra paint can tips is a great idea. The only down side is the small corner wheel. would not stay in place without tightening the thumb nut with pliers. the small nubs are not large enough to keep the wheel in place.

Is this review helpful?

Vers A Striper

Your review: Good little machine for the price. Did what I needed to do.

Is this review helpful?

Economical

Your review: Very good Line Striper for a fair price.

Is this review helpful?

Sort by: 
1 2 ...

28 Results

Be the First to Ask a Question!