Belt Kit for Telescoping Wands

Rollover image to zoom in

Click image to enlarge

See all 14 items in product family

Belt Kit for Telescoping Wands

Item #: WBB187096

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $22.50
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Belt Kit for Telescoping Wands

Used to support Long Wands, taking stress off the arms and body. For use with all Long Wands. Adjustable to fit any size.

Product Specifications

    • COLOR FINISHBlack
    • BRANDBE Pressure
    • MANUFACTURERS PART NUMBER85.400.019
    • SIZE TYPEAdjustable

Avg. Customer Rating: (5 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating

Belt definitely helps

Helps relieve stress on your back especially when the wand is exteneded to maximum lengths.

See more critical reviews

Sort by: 

5 Results

Belt

Your review: If you have or buy the wand, get this belt. Hands down a great help to take the weight of the job.

Pros: Easy to adjust, good fit

Cons: Could use a pad on the strap around the neck. I added my own

Is this review helpful?

A must have for a telescoping wand

Your review: This belt is a must have when using a telescoping wand. I would have given it 5 stars but the grommet on the pole attachment came off the nylon strap. I had to put a bigger grommet on it and use a couple of washers to fix it. I was surprised that belt will even accommodate a 50" waist.

Pros: Fits XL waists. Supports the wand for long use.

Cons: Grommet came off. Bolt on the pole clamp could be shorter.

Is this review helpful?

Belt definitely helps

Your review: I have no problem with the belt, it works as designed. The problem is with the directions and location of the pressure washer handle itself. I was getting no assistance from the belt while following the provided instructions. I finally made the decision to loosen the pressure washing handle and slide it up the tubing. Once I did this, it made the belt more effective and the wand easier to manipulate while relieving some stress on my back.

Pros: Helps relieve stress on your back especially when the wand is exteneded to maximum lengths.

Cons: Directions are not very good. I had to figure out what worked best. The suggestion here is to make the directions more clear. and relocate the wand handle closer to your body to relieve the stress on your back.

Is this review helpful?

Handed Belt

Your review: This belt is so needed to operate the telescopic wand without it i believe that at some giving time you would have the ability to loss control of the 24ft. wand.

Is this review helpful?

Telescoping Wand Belt

Your review: I have only used it once since I purchaced the belt. But I used it for about 7 or 8 hours pressure washing my daughters school. It worked just like expected. Gave the weight off my arms and made it easy to work the wand. Would recommend to anyone with a Telescoping wand.

Is this review helpful?

Sort by: 

5 Results

There are 5 questions and 1 answers for this product.

Sort by: 

5 Results

Will this product fit a Shark RG 2.5 @ 3000 Honda Gc190 Gas Cold Water Direct Drive Pressure Washer?? Or would I also have to purchase an adapter? It says that it has M22 threads but does my Honda GC190 also hav M22 threads?

Question Asked By: Will , April 30, 2012

+ View 1 Answer

Answer This Question

Sort by: 

5 Results

SAVE BY EMAIL

Exclusive Offers, Weekly Deals!

C&H Government Buyers
Call Us
1.888.978.7759
Chat Online

54.146.169.191:66