Ice Buster Walk Behind Salt Spreader - 3021309

Rollover image to zoom in

Click image to enlarge

See all 12 items in product family

Ice Buster Walk Behind Salt Spreader - 3021309

Item #: WB640189

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $189.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
ICE BUSTER WALK BEHIND SALT SPREADER

Ice Buster salt spreader has an all-welded steel frame and large 1.5 cu. ft. polymer hopper with screen that helps prevent material jamming. Ice Buster has 100 lb. capacity and features large 13" diameter pneumatic tires that make pushing through slush and ice easy. Comfort grip handle has a large flow regulator for ease-of-use. Heavy-duty gearbox for long life. The commercial grade alloy gears are now fully enclosed, protecting the integrity of the gears from salt, weather, and rust. A built-in flow regulator allows you to control the amount of material used with incredible precision. Adjustable Spread Radius 3' to 30'. Zinc-plated steel axle, agitator shaft and linkage offer reliable corrosion resistance that withstands extreme temperatures. Salt spreader has a 3-flap adjustable poly deflector that controls spread pattern, and a rear deflector protects operator's feet. Includes plastic rain cover to protect contents from the elements. Blue color finish. Easy assembly.

Product Specifications

    • LENGTH INCHES40
    • WIDTH INCHES26
    • HEIGHT INCHES31
    • CAPACITY LBS100
    • COLOR FINISHBlue
    • APPLICATIONIce Melt, Salt, Seed, Fertilizer, Lime
    • ASSEMBLYUnassembled
    • BRANDIce Buster
    • CONSTRUCTIONPlastic Hopper/Steel Frame
    • MANUFACTURERS PART NUMBERIB100B
    • STYLEAdjustable Spread Radius 3' to 30'
    • TYPEWalk Behind Spreader
    • WEIGHT LBS42
    • WHEEL DIAMETER INCHES13
    • SPREADER TYPEWalk Behind
Have A Question About This Product?
1 Question | 1 | Answer

Avg. Customer Rating: (25 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Heavy Duty Salt Spreader

Holds two bags of salt and easy to handle. Salts breaks up. Adjustable deflectors for throw path

See more favorable reviews

The most critical review

  • Customer Rating

Did not last long

They looked great out of the box and shipping was fast. Assembly was fast and easy. Price was great.(We purchased 6)

See more critical reviews

Sort by: 
1 2 ...

25 Results

Heavy Duty Salt Spreader

Your review: We had been using heavy duty fertilizer spreaders in the past, but they would clog up so easily. This spreader is a beast and never clogs. Easy to push and manuver. Quickly covers a lot of area and well built.

Pros: Holds two bags of salt and easy to handle. Salts breaks up. Adjustable deflectors for throw path

Cons: Could use a better agitator

Is this review helpful?

Love these

Your review: I work for a company that uses these all over our site and they are perfect for what we need them for.

Pros: Compact enough to get in tight spaces.

Cons: Could use a better comfort handle

Is this review helpful?

Salt Spreader

Your review: Very nice made and worth the money.

Pros: Very well made. Looks great.

Cons: Directions not very user friendly and a little difficult to put together.

Is this review helpful?

Salt Spreader

Your review: Just purchased 2 of these units and they work great. The capacity of the hopper allows to cover more area in less time because we don't have to stop as much to refill with salt.

Pros: Big capacity hopper, Rubber tires make for easy mobility on snow and ice, ergonomic handle makes for less back strain while pushing the unit, adjustable spread pattern means less wasted salt.

Cons: none that I see at this time

Is this review helpful?

salt spreader

Your review: well built. looking forward to years of service

Pros: easy to maneuver

Cons: none noted

Is this review helpful?

Ice Spreader

Your review: Does a good job spreading ice and keeping the top covered so it doesn't clump.

Pros: Cost efficient and quality product

Cons: none

Is this review helpful?

ice busterwalk behind salt spreader

Your review: vey satisfied thank you

Is this review helpful?

Did not last long

Your review: We saved a few bucks by purchasing these, they lasted through Dec and most of Jan. They are not the best quality but they may work great for small operations. Not recommended for major snow removal companies.

Pros: They looked great out of the box and shipping was fast. Assembly was fast and easy. Price was great.(We purchased 6)

Cons: The valve stem separated from the inner tube on several units, the plastic feed control broke loose from the bottom and you can not fix this. The gears lock up frequently, the salt deflectors are always loose and moving around. The agitator pin rubs against the plastic on the bottom black plastic. The control often slips open allowing for product to come out.

Is this review helpful?

BUILDING MANAGER First Congregational Church UCC

Your review: GREAT ....

Is this review helpful?

Salt spreader

Your review: Great product, performs perfect and is heavy built.

Is this review helpful?

purchased products

Your review: Products were delivered on time and complete.

Is this review helpful?

ICE BUSTER

Your review: We have purchased >6 of these units in the past and I feel like these new ones have gone thrue and cost of material control process because these feel to be lighter weight such as thinner steal and also the handles have a slight twist in them because the holes pressed from manufacturing are not square. AND, the axle sprocket feels and sounds like it is going to lock up when in motion. The two pieces seem to be spaced apart a little differently. I purchased Ice buster because the last group of them lasted maybe 2 seasons and that is not bad for washing after use. I feel the gears will lock up on these new ones before I have corrosion issues. I gave 3 stars for the Price I paid.

Is this review helpful?

Salt spreader

Your review: Very pleased with spreader does exactly what was needed.

Is this review helpful?

Excellent spreader!

Your review: Purchased for city sidewalks that are shaded by condo building and constantly thaw and refreeze. Very sturdy, works great, much more even distribution of the ice melt. Walks seemed to stay clear longer. I ordered and it was here within 24 hours. Wow! I have already recommended to others.

Is this review helpful?

Walk Behind Salt Spreader

Your review: Very sturdy spreader. We have been using them for about 3 years now. Recently purchase more to upgrade fleet.

Is this review helpful?

Ice buster

Your review: Quality looks to be of good grade. Haven't used it yet so we don't know how the functionality is, yet. Like the anti-clogging grate at the bottom of the bucket to separate the salt is it enters the spreader area. We will see how it holds up.

Is this review helpful?

Ice buster

Your review: This is a great product so far. It is sturdy and well built. The all metal gear and big tires are just what is needed for the sloppy icy snow we are getting right now in MN. This spreads well and quickly. The only problem I have is the control for the flow sometimes starts to open on it's own as the nut that hollds it on doesn't stay tight. I have solved this with a layer of teflon tape over the threads.

Is this review helpful?

Does a Nice Job !

Your review: The spreader works well except for the release lever for the salt. Could be made a little bit better.

Is this review helpful?

1 person found this review helpful

Great Product

Your review: Works well the control on the spreader is the best I have used. The salt deflecter could be a little stronger.

Is this review helpful?

Salt spreader

Your review: I would buy another if needed.

Pros: does a great job

Cons: none that i know

Is this review helpful?

ice buster walk behind salt spreader

Your review: Like the product, handle could be bolted together better. When assembled you can feel play in the handle. Left to right and the reverse.

Is this review helpful?

NICE ICE BUSTER....

Your review: The machine spreads nicely, I used it around an area of about 24 parking spots. Its seems to be built well. If we take care of it, I hope it lasts for a while.

Is this review helpful?

Salt Spreader

Your review: Well built spreader, looking foward to using it the first snowfall

Is this review helpful?

ICE Buster

Your review: A solid piece of equipment. Works exactly as advertised.

Is this review helpful?

Sort by: 
1 2 ...

25 Results

There are 25 questions and 1 answers for this product.

Sort by: 
1 2 ...  

25 Results

how come you dont sell any relpcement parts for the salt spreader i have 2 parts that broke and i cant use the spreader

Question Asked By: Richard , pennsylvania , February 04, 2015

+ View 1 Answer

Answer This Question

Sort by: 
1 2 ...  

25 Results

No Thanks x
Save $25.00 with this comparable product +
Item #: WB640788
globalindustrial.com
Ships same day.
$164.95
SAVE BY EMAIL

Exclusive Offers, Weekly Deals!

C&H Government Buyers
Call Us
1.888.978.7759
Chat Online

54.197.151.150:62