Elkay, Wall Mounted Drinking Fountain, Bracket Style, Stainless Steel, EDF15R

Rollover image to zoom in

Click image to enlarge

See all 4 items in product family

Elkay, Wall Mounted Drinking Fountain, Bracket Style, Stainless Steel, EDF15R

Item #: WBB190520

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $394.00 Save up to 43%
Price: $ 224.95

Frequently Purchased Together

Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Elkay - BRACKET FOUNTAINS - EDF15R

Number 300 Series, nickel bearing satin finish stainless steel drinking fountain has a contoured basin to eliminate splashing and standing water, and a 14 gauge, heavy duty wall bracket. Basin has rounded corners for added safety and ease of maintenance, and a removable chrome-plated strainer.

Image May Not Reflect Selected Options


Documents are in PDF format

Product Specifications

    • ADA CERTIFIEDNo
    • ANSI CERTIFIEDYes
    • BASIN DEPTH INCHES3
    • BRANDElkay
    • BUBBLERPush Button
    • COLOR FINISHStainless Steel
    • DEPTH INCHES6
    • FILTERNo
    • FREEZE/FROST RESISTANTNo
    • GLASS FILLERNo
    • HEIGHT INCHES8-3/8
    • INSTALLATION TYPEWall
    • MANUFACTURERS PART NUMBEREDF15R
    • NSF CERTIFIEDYes
    • NUMBER OF STATIONS1
    • REFRIGERATEDNo
    • VANDAL RESISTANT BUBBLERNo
    • WIDTH INCHES10
    • INCLUDES--
    • FOR OUTDOOR USENo
Have A Question About This Product?
0 Question | 0 | Answer

Avg. Customer Rating: (15 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating

Can't stop the leaking

I bought wall mounted drinking fountain it leaked from the start. I took it apart and put plumbers putty and Teflon with still leaked.

See more critical reviews

Sort by: 
1 ...

15 Results

Just as pictured

Your review: Only problem I have with fountain is that the connection is an odd size. I had buy a fitting to convert it in order to connect with supply line.

Pros: Super fast shipping

Cons: supply fitting size.

Is this review helpful?

Mr

Your review: Excellent product!!

Pros: Durable!

Cons: none

Is this review helpful?

Oh well

Your review: Everything was just fine as for the product and how fast I received it. The only problem I have is the cost of the product. Not too many people sell those but I don't agree that this cost as much as I paid.

Pros: Good service

Cons: Too expensive

Is this review helpful?

Can't stop the leaking

Your review: I bought wall mounted drinking fountain it leaked from the start. I took it apart and put plumbers putty and Teflon with still leaked.

Is this review helpful?

Elkay, Wall Mounted Drinking Fountain, Bracket Sty

Your review: In the proper application, where you need a compact drinking fountain, this product is perfect. You can face it any direction so that the approach to the fountain is not an issue either. Great value for the cost.

Is this review helpful?

wall mounted fountain

Your review: Great price and quick delivery on this fountain for our pool area. Needed an adaptor for the hose hook-up but was easy to find at Home Depot. Works great.

Is this review helpful?

Sink purchase

Your review: My purchase of a wall mounted water fountain was great. It was easy to purchase, inexpensive and very intuitive.

Is this review helpful?

Elkay Wall Mounted Drinking Fountain

Your review: This water fountain serves the purpose just right. Doesn't take up a lot of space on the wall, it's affordable, easy to install that even a monkey could do it, and if you need a filter then easy just to add in an inline just before you get to the fountain. Would recommend if you are looking for a compact and affordable drinking station.

Is this review helpful?

DISAPPOINTMENT

Your review: THIS FOUNTAIN WAS A LET DOWN TO SMALL. I HAD PURCHASE IT FOR OUR FAMILY LIFE CENTER. WHEN REVIEWING ON INTERNET IT APPEARS LARGE. I REALIZE THAT THIS FOUNTAIN ALSO DID NOT HAVE A COOLING ELEMENT TO KEEP THE WATER COLD.

Is this review helpful?

Sometimes less is more!!!

Your review: These fountains were super easy to install, and they look great at our pool. They were exactly what we needed. Thanks for providing a quality product. I would definitely recommend you to a friend.

Is this review helpful?

Bracket Fountain WBB190520

Your review: great item for small establishment, better still if water hose connecting hardware comes together

Is this review helpful?

Wall mount water fountain

Your review: Very nice product, easy to install the bracket, the only problem is the water connection, connector is not included so I went to home depot and there is no water line that fit on this. So I bought some connector and fitting to make it work. UNtil now customer is satified.

Is this review helpful?

Elkay Bracket Fountain, functional and inexpensive

Your review: This Elkay fountain is extremely well made and easily modifiable for unusual applications. Global Industrial had the best price by far! If I needed a dozen more, I would stick with this product.

Is this review helpful?

Just in Time!

Your review: Purchased this water fountain from Globalindustrial.com just before the start of swim season at our community pool. It was shipped and received on time and was exactly as expected. It is a very basic fountain but Global's price was better than competitors and included free shipping making this fountain a real value. It isn't fancy but fulfills our requirements for a fountain at the pool and should provide years of service.

Is this review helpful?

fountain

Your review: it works well, the specifications could be better as to what you will need to install this product.

Is this review helpful?

Sort by: 
1 ...

15 Results

Be the First to Ask a Question!