Relays
Type
Number Of Relays
Voltage
Brand
Features
Certifications
Length
Mounting Location
Width
Depth
Height
Color
Price
Related Products
RIB® Enclosed Latching Relay RIBL24SBM, 20A, 24VAC/DC, W/switch & Aux Contact The Latching Series comes prepackaged in their own NEMA 1 plastic enclosure with a 1/2" mounting nipple, LED indicator and pre-wired for a money-saving installation that is easy and quick. These relays are activated by pulse commands from a controller or momentary switch closure. The relay contacts are mechanically latched in the closed position and the load will remain on in the event of a control panel failure period. If power is completely lost the contacts will remain in their last state and the load will ...
RIB® BACnet, LonWorks, and Ethernet Network Compatible Devices can be hard wired and used instead of more expensive multi-output controllers when a few more control points are needed, and large controllers are too much for the job. They can also be used when control points are widely spread throughout the job site. These devices have been prepackaged to save the installer the time, trouble, and expense of buying separate components and assembling them on the job. Functional Devices also offers WiFi, Zigbee, AIC, and EnOcean WIRELESS Network Compatible Devices that can act singly as a ...
RIB® Enclosed Latching Relay RIBL24SB, 20A, 24VAC/DC, W/switch The Latching Series comes prepackaged in their own NEMA 1 plastic enclosure with a 1/2" mounting nipple, LED indicator and pre-wired for a money-saving installation that is easy and quick. These relays are activated by pulse commands from a controller or momentary switch closure. The relay contacts are mechanically latched in the closed position and the load will remain on in the event of a control panel failure period. If power is completely lost the contacts will remain in their last state and the load will activate upon the ...
The Latching Series comes prepackaged in their own NEMA 1 plastic enclosure with a 1/2" mounting nipple, LED indicator and pre-wired for a money-saving installation that is easy and quick. These relays are activated by pulse commands from a controller or momentary switch closure. The relay contacts are mechanically latched in the closed position and the load will remain on in the event of a control panel failure period. If power is completely lost the contacts will remain in their last state and the load will activate upon the return of normal power or emergency power.
RIB® BacNet Enclosed Relay RIBTW24B-BCAI, 20A, SPDT, 24VAC/DC, Analog In RIB® BACnet, LonWorks, and Ethernet Network Compatible Devices can be hard wired and used instead of more expensive multi-output controllers when a few more control points are needed, and large controllers are too much for the job. They can also be used when control points are widely spread throughout the job site. These devices have been prepackaged to save the installer the time, trouble, and expense of buying separate components and assembling them on the job. Functional Devices also offers WiFi, Zigbee, AIC, and ...