Air Curtains 101: How They Work, Where to Use Them & How to Size One

Key Takeaways:

 

  • Air curtains create an invisible barrier of moving air across door openings to help separate indoor and outdoor environments.
  • They can help reduce energy loss, improve temperature control, and limit the entry of dust, insects, and airborne contaminants.
  • Air curtains are commonly used in warehouses, loading docks, restaurants, retail stores, healthcare facilities, and food-processing operations.
  • Proper sizing depends on doorway height, width, mounting location, and environmental conditions.
  • Heated and unheated models serve different purposes and should be selected based on the facility's needs.

 

An air curtain is a mechanical device that creates a controlled stream of air across an open doorway or entrance. Although invisible, this airflow acts as a barrier that helps reduce the exchange of air between two environments.

 

Unlike a physical door, an air curtain allows people, equipment, and products to move freely while helping maintain indoor conditions. This makes air curtains especially valuable in facilities where doors open frequently throughout the day.

 

Air curtains are often installed above entryways, loading docks, drive-through windows, receiving areas, and service counters where maintaining separation between indoor and outdoor conditions is important. They are also widely used in foodservice and food-processing environments, particularly at the entrances to walk-in freezers, refrigerators, and meat lockers, where controlling temperature and limiting contamination are critical to both food safety and energy efficiency.

 

How Do Air Curtains Work?

 

Air curtains use high-velocity airflow to create a protective barrier across an opening.

 

When properly sized and installed, the air stream helps prevent outdoor air from entering the building and reduces the loss of conditioned indoor air. This can help maintain more consistent temperatures and reduce the workload placed on heating and cooling systems.

 

Air curtains can also help block:

 

  • Dust and debris
  • Flying insects
  • Vehicle exhaust
  • Airborne contaminants
  • Humidity

 

While they are not airtight seals, they can significantly reduce environmental transfer when compared to an open doorway without protection.

 

Why Businesses Use Air Curtains?

 

Many facilities install air curtains primarily for energy savings, but the benefits often extend much further.

 

In warehouses and distribution centers, air curtains help reduce temperature fluctuations at loading docks where doors may remain open for extended periods. In restaurants and food-service operations, they can help minimize insect intrusion and support more consistent indoor temperatures.

 

Retail stores frequently use air curtains at customer entrances to improve comfort during both summer and winter months. Healthcare facilities and food-processing operations may use them as part of broader environmental control and sanitation strategies.

 

The result is often a combination of improved comfort, lower strain on climate control systems, and better environmental control throughout the facility.

 

Common Air Curtain Applications

 

Air curtains can be found across a wide range of commercial and industrial environments.

 

Facility Type Common Application
Warehouse Loading docks, shipping doors, receiving areas
Distribution Center Dock doors and material handling entrances
Restaurant Customer entrances, kitchen service doors, drive-through windows
Retail Store Main entrances and receiving doors
Food Processing Facility Environmental separation and contamination control
Healthcare Facility Entrances and controlled environments
Commercial Building Lobbies, vestibules, and high-traffic entrances

 

 

Because they can be installed in both conditioned and unconditioned spaces, air curtains are often used anywhere frequent door openings create operational challenges.

 

Do Air Curtains Save Energy?

 

One of the most common reasons organizations invest in air curtains is to reduce energy loss.

 

Every time a door opens, conditioned air escapes as outdoor air enters the building. During summer months, hot air and humidity can infiltrate indoor spaces. During winter, heated air is lost while cold air enters.

 

Air curtains help reduce this air exchange, allowing heating, ventilation, and air conditioning (HVAC) systems to operate more efficiently. Savings vary by facility and usage patterns, but reducing the infiltration of unconditioned air can lower heating and cooling demands as well as maintain more stable indoor temperatures.

 

Facilities with high-traffic entrances or frequently opened dock doors often see the greatest benefits.

 

Heated vs. Unheated Air Curtains

 

One of the most important purchasing decisions involves choosing between a heated and an unheated unit.

 

Type Best For Primary Benefit Considerations
Unheated Air Curtain Most commercial and industrial applications Controls air exchange and improves efficiency Lower operating costs
Heated Air Curtain Cold climates and customer-facing entrances Provides supplemental warmth and comfort Higher energy consumption

 

Unheated air curtains are often sufficient for warehouses, loading docks, and industrial environments where the primary goal is reducing unconditioned air infiltration.

 

Heated air curtains are commonly used at retail entrances, hospitality facilities, and other customer-facing locations where occupant comfort is a higher priority.

 

Air Curtains and Food-Service Applications

 

Restaurants, commercial kitchens, and food-service facilities often face unique environmental challenges.

 

Frequent deliveries, employee traffic, and customer entrances can create opportunities for insects, dust, and outdoor air to enter the building. Air curtains help create a protective barrier that supports cleaner indoor environments and reduces temperature fluctuations.

 

Many food-service operators use air curtains above service doors, receiving entrances, walk-in freezers/refrigerators at food-processing facilities, and drive-through windows to improve operational efficiency and environmental control.

 

Because compliance requirements vary by jurisdiction and facility type, operators should always verify local health and building code requirements when evaluating air curtain installations.

 

How to Size an Air Curtain

 

Proper sizing is critical to air curtain performance.

 

A unit that is too small may fail to create an effective barrier, whereas an oversized unit can increase operating costs without delivering additional benefits.

 

The most important sizing factors include doorway width, doorway height, mounting location, and environmental conditions. In general, the air curtain should span the full width of the opening and provide sufficient airflow velocity to reach the floor or intended coverage area. Wider openings may require multiple units or specially designed systems to ensure complete coverage across the entire opening.

 

Air Curtain Sizing Guidelines

 

Door Height Typical Consideration
Up to 8 ft Standard commercial entrances
8–12 ft Retail, restaurants, and light industrial spaces
12–16 ft Warehouses and receiving areas
16 ft+ High-bay industrial and distribution applications

 

Because airflow performance varies by manufacturer and application, buyers should always review product specifications before making a final selection.

 

Installation Considerations

 

Successful air curtain performance depends on more than equipment selection alone.

 

Installation height, mounting position, airflow direction, and surrounding environmental conditions all determine effectiveness. Facilities should also consider electrical requirements, maintenance access, and whether the unit will operate continuously or only when doors are open.

 

In high-traffic industrial environments, integrating air curtains with door controls can help automate operation and maximize efficiency.

 

Air Curtains Can Improve Comfort, Efficiency & Environmental Control

 

Air curtains offer a practical solution for facilities looking to reduce energy loss, improve temperature control, and limit the movement of contaminants through frequently used openings.

 

Whether installed at a warehouse loading dock, restaurant entrance, retail storefront, or food-processing facility, a properly selected and sized air curtain can help support HVAC performance while creating a more comfortable indoor environment.

 

For organizations evaluating climate-control strategies, air curtains are often one of the most cost-effective ways to improve building performance without restricting access or workflow.

 

Frequently Asked Questions

 

Do air curtains actually work?

 

Yes. When properly sized and installed, air curtains can significantly reduce the exchange of indoor and outdoor air. They also help control temperature, humidity, insects, and airborne contaminants.

 

Do I need a heated air curtain?

 

Not necessarily. Many warehouses, loading docks, and industrial facilities use unheated air curtains successfully. Heated models are most often selected when occupant comfort is a priority, particularly at customer-facing entrances in colder climates.

 

Can an air curtain replace a door?

 

No. Air curtains are designed to supplement doors, not replace them. They help reduce air exchange when doors are open but do not provide the security, insulation, or weather protection of a closed door.

 

Where should air curtains be installed?

 

Air curtains are typically mounted above doorways, loading docks, drive-through windows, service entrances, and other openings where environmental separation is important.

 

How do I know what size air curtain I need?

 

The most important factors are doorway width, doorway height, mounting location, and the environmental conditions on each side of the opening. The unit should provide full coverage across the opening and sufficient airflow to create an effective barrier.

 

The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes, and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.