7 Types of Commercial Outdoor Seating

Well-chosen outdoor seating enhances guest comfort, encourages longer visits, and reduces upkeep costs. Hospitality and commercial properties that invest in modular, low-maintenance outdoor furnishings often see higher guest satisfaction and increased dwell time. Property owners and managers typically prioritize durability, weather resistance, comfort, ease of maintenance, and code compliance, especially in high-traffic or public areas.

 

Below are seven proven types of commercial outdoor seating, each suited to different aesthetics, climates, and operational requirements:

 

  • Recycled HDPE plastic benches
  • Thermoplastic-coated metal chairs & benches
  • Teak & hardwood outdoor seating
  • Concrete seating
  • Synthetic HDPE wicker furniture
  • Stackable resin café chairs
  • Modular cushioned lounges and booths

 

Each option offers distinct advantages in durability, maintenance, and visual appeal, making it easier to match seating solutions to your facility’s environment and usage needs. Global Industrial provides code-compliant, weather-resistant options with ready-to-ship availability, helping you create outdoor spaces that are both functional and welcoming.

 

For a broader overview of materials and product categories, explore Global Industrial’s outdoor seating selection.

 

Accessibility Requirements

 

Adhering to accessibility requirements when choosing outdoor furniture is important because it ensures that outdoor spaces are compliant with the Americans with Disabilities Act (ADA) while being welcoming, usable, and safe for everyone. To meet ADA guidelines, furniture must have adequate clearance for mobility devices and provide stable seating with appropriate heights, and it cannot obstruct pathways. This helps to prevent exclusion and physical barriers that can limit enjoyment of patios, parks, or commercial outdoor areas. Beyond inclusivity, ADA-compliant furniture can improve overall comfort and navigation for all users, from older adults to families with strollers, while also helping property owners reduce liability risks and demonstrate a commitment to accessibility, equity, and thoughtful design.

 

Things to consider when choosing & laying out furniture to create outdoor spaces include:

 

  • ADA-compliant table and seat heights, reach ranges, and clear pathways
  • Plan placement for accessibility, guest flow, and staff movement
  • Arrange modular furniture sets to maintain accessibility
  • Ensure at least 5% of seating is wheelchair accessible
  • ADA-compliant table heights, reach ranges, and turning radius

 

The information offered here provides general guidelines for compliance. For full details on the ADA and to ensure complete compliance, visit ada.gov.

 

Recycled HDPE Plastic Benches

 

Recycled high-density polyethylene (HDPE) benches combine sustainability with commercial durability. HDPE resists moisture, impact and ultraviolet radiation (UV) exposure while requiring minimal upkeep. These benches are ideal for parks, campuses, and healthcare entrances where reliability and sanitation matter.

 

Key Advantages:

 

  • Won’t rot, rust, or attract insects
  • Extremely durable and impact-resistant
  • Low-maintenance and easy to clean

 

Placement Guidelines:

 

  • Consider anchoring in windy or high-traffic areas

 

Thermoplastic-Coated Metal Chairs and Benches

 

Thermoplastics are applied in a similar fashion as a conventional hard powder coat, but melt and flow without a chemical reaction. This results in a thicker, softer, and repairable finish. Being thicker & softer makes it more comfortable to sit and lean on, it remains a comfortable temperature even in high heat & direct sunlight, and since it's repairable the furniture will stay in service longer.

 

Thermoplastic-coated steel or galvanized finishes deliver stability, durability, and a clean, modern look. With basic care, steel park benches last 20–30 years and provide weight for security and theft deterrence.

 

Key Advantages:

 

  • Heavy-gauge frames and anchorable bases resist tampering
  • Long service life reduces the need for refinishing
  • Low-maintenance and easy to clean

 

Placement Guidelines:

 

  • Use anchoring or weighted bases in windy or public areas

 

Teak & Hardwood Outdoor Seating

 

Teak is a dense hardwood with natural oils that repel moisture and pests, making it inherently weather resistant. Wood furniture offers a warm, classic look and comfort, but requires more upkeep than synthetics. Untreated teak gradually develops a silver patina; periodic oiling or sealing preserves a golden tone.

 

Key Advantages:

 

  • Naturally resistant to rot and insects
  • Strong, long-lasting, and visually appealing
  • Develops an attractive patina over time

 

Placement Guidelines:

 

  • Consider shade, sunlight exposure, and spacing for comfort

 

Concrete Seating

 

Precast concrete seating provides permanence, tamper resistance, and minimal maintenance—ideal for municipalities, campuses, and security-sensitive sites. Its mass and durability deter theft and vandalism.

 

Key Advantages:

 

  • Extremely durable and long-lasting
  • Tamper-resistant and heavy to deter theft
  • Minimal upkeep required

 

Placement Guidelines:

 

  • Seats are heavy and cannot be easily moved, so plan placement carefully
  • Curved profiles and nearby shade improve comfort

 

Synthetic HDPE Wicker Furniture

 

Synthetic HDPE wicker mimics handwoven rattan with UV stability, colorfastness, and tensile strength. Lightweight & low maintenance, it’s ideal for hospitality, pool decks, and lounge areas. Pair frames with mildew-resistant, quick-dry cushions and solution-dyed fabrics to preserve color in sunny environments.

 

Key Advantages:

 

  • Lightweight yet durable for long-term outdoor use
  • Resists corrosion and fading in direct sunlight
  • Comfortable when paired with outdoor-grade cushions

 

Placement Guidelines:

 

  • Consider shade, sunlight exposure, and spacing for guest comfort

 

Stackable Resin Café Chairs

 

Resin seating is molded for strength, UV stability, and all-weather performance. Chairs that nest or stack provide affordability, portability, and easy storage. These designs also make daily setups and takedowns faster and more efficient.

 

Key Advantages:

 

  • Non-corrosive and weather-resistant
  • Stackable or nestable for convenient storage and portability
  • UV-inhibited versions resist color fading

 

Placement Guidelines:

 

  • Arrange for staff access and safe guest flow

 

Snapshot: HDPE benches vs. alternatives

 

Material

Weather Resistance

Maintenance

Typical Lifespan

Vandal/Impact Resistance

Best-use Scenarios

Recycled HDPE

Excellent vs. rain, salt, UV

Soap/water; no sealing

25–40 years

High; won’t rot or splinter

Parks, campuses, healthcare

Thermoplastic-coated steel

Excellent if coating intact

Periodic wash; inspect finish

20–30 years

Very high; anchorable

Urban sidewalks, transit, schools

Teak/Hardwood

Naturally good; needs care

Clean; oil/seal as desired

10–20 years

Moderate; can dent/scratch

Hospitality patios, terraces

Concrete

Extremely durable

Minimal; clean as needed

30+ years

Very high; tamper resistant

Municipal/public spaces

Commercial resin

Good with UV-s table grades

Hose off; mild cleaners

Varies by grade

Moderate; lighter weight

Seasonal cafés, pop-ups

 

 

Modular Cushioned Lounges and Booths

 

Modular seating systems can be reconfigured, scaled, or repaired as needs change, making them ideal for hospitality and multi-use campuses. Comfortable seating encourages longer stays and improves guest satisfaction, especially when designed with ergonomic frames and supportive cushions.

 

Key Advantages:

 

  • Reconfigurable and scalable to fit different layouts
  • Comfortable, ergonomic cushions encourage longer stays
  • Durable frames designed for high-traffic areas

 

Placement Guidelines:

 

  • Consider shade, sunlight exposure, and spacing for guest comfort

 

Choosing Weather-Resistant Materials

 

Materials are engineered to handle rain, UV exposure, temperature swings, and humidity without fading, rusting, or warping. Aluminium, teak, synthetic wicker, and recycled plastic balance weight, durability, and care demands. Solution-dyed acrylics, like Sunbrella, are fade-resistant and water-repellent for cushions and umbrellas.

 

Quick comparison of weather-ready materials:

 

Material

Best Climate

Corrosion/Rot Resistance

UV/Color Stability

Maintenance

Notes

Recycled HDPE

Wet, coastal, freeze–thaw

Won’t rot or rust

Very good

Low

Heavy, durable, cleans easily

Thermoplastic-coated steel

Temperate/Windy

Excellent if coating is intact

Very good

Low–moderate

Anchorable, strong vandal resistance

Aluminum

Humid/Coastal

Won’t rust; may oxidize

Very good

Low

Light, easy to move; add ballast in windy sites

Teak/Hardwoods

Temperate/Sunny

Naturally rot resistant

Good; patinas

Moderate

Periodic cleaning and optional oil/seal

Synthetic HDPE wicker

Sunny

Non-corrosive

Very good

Low

Pair with outdoor-grade cushions

Commercial resin

Seasonal

Non-corrosive

Good with UV inhibitors

Low

Stackable; check commercial rating

 

 

Balancing Comfort, Durability, and Maintenance

 

Ergonomic designs improve guest satisfaction and reduce discomfort, supporting longer stays. Low-maintenance furnishings free staff for faster service. Modular, repairable pieces reduce downtime by allowing component swaps instead of full replacements.

 

Planning Layout, Safety, and Regulations

 

Map your space for guest movement, accessibility, and security. Verify sidewalk seating permits and setback requirements. Ensure at least 5% of outdoor tables are wheelchair accessible (ADA guidance) and maintain clear pedestrian routes.

 

Layout and Regulatory Guidelines:

 

  • Sidewalk and fire lane clearance
  • ADA table heights, reach ranges, and turning radius
  • Anchoring or weighted bases in windy or public areas
  • Lighting, shade, proximity to power, heaters, and host stands
  • Staff movement for service and bussing

 

Frequently Asked Questions

 

What materials are best for commercial outdoor seating in wet climates?

 

HDPE, thermoplastic-coated metals, and teak resist moisture, rot, and corrosion, providing reliable year-round performance.

 

How can I maintain and protect outdoor seating to extend its lifespan?

 

Clean regularly, inspect finishes and hardware, and use manufacturer-recommended treatments or covers. Prompt repairs prevent minor issues from becoming major problems.

 

What should I consider when selecting cushioned outdoor furniture?

 

Choose solution-dyed, mildew- and fade-resistant fabrics with quick-dry foam, and prioritize removable, washable covers for easy care.

 

How does material choice affect total cost of ownership?

 

Durable materials like recycled plastic or thermoplastic-coated steel may cost more upfront but reduce refinishing, repairs, and replacement over time.

 

Are there features to enhance vandal resistance in public seating?

 

Opt for heavy, anchorable designs such as concrete or steel benches, and specify tamper-resistant hardware.

 

The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.