Battery-powered tools are now achieving and even surpassing traditional, gas-powered equivalents. The commercial-grade tool industry that was once dominated by gas-powered and tethered tools is now increasingly led by battery-powered options. With top-notch power and safety, these eco-friendly tools have reached a level of performance that meets and often exceeds their gas-powered counterparts. Plus, the rechargeable aspect of battery-powered tools add a level of convenience and versatility unmatched by gas powered and tethered counterparts. Thanks to advancements in technology - particularly in lithium batteries - battery tools now offer industrial grade performance.
The Rise of Cordless Power Tools and Battery Platforms
The widespread adoption of battery tools, once met with skepticism, is now transforming industries thanks to groundbreaking advancements in battery technology by leading brands. Companies like Milwaukee, Makita, Flex, and DeWalt/Black & Decker have invested heavily in research and development, integrating cutting-edge battery systems into their product lines, creating tools that not only match but often surpass the performance of gas-powered equipment in terms of power, reliability, and convenience.
Milwaukee has set a high standard with its dual battery platforms: the M18 and M12 systems. The M18 platform is designed for heavy-duty applications, offering superior torque and extended battery life for larger tools, while the M12 line is more compact, providing a balance of portability and power for smaller tasks. Both platforms feature advanced REDLITHIUM battery technology, known for its durability, longer run times, and ability to perform in extreme temperatures, making them versatile for a wide range of job sites.
Makita's LXT series also stands out by offering over 300 tools that operate on the same 18V battery platform. This cross-compatibility simplifies the user experience, allowing workers to switch between tools without the hassle of different battery types. Makita’s STAR Protection Computer Controls further enhance battery safety and performance by protecting against overloading, over-discharging, and overheating, ensuring longer battery life and consistent power delivery.
While many cordless tools offer convenience, Flex tools are equipped with high-capacity lithium-ion batteries that deliver longer run times and faster charging than most competitors. They maintain consistent power even under heavy loads, making them more reliable for demanding tasks. The Flex Max Lithium Ion battery combines intelligent battery management with Therma-Tech™ cooling technology to deliver a driving force that's up to 20% higher than anything you've already seen out there.
DeWalt's FLEXVOLT system adds another layer of innovation by introducing a flexible battery platform that adjusts between 20V and 60V, depending on the tool's requirements. This versatility allows users to tackle both light and heavy-duty tasks with a single battery, seamlessly switching from cordless to corded operation when higher power is needed. The FLEXVOLT system ensures that users have the right level of performance for any job, reducing downtime and enhancing overall productivity.
The Battery: The Game Changer
At the heart of the battery tool revolution is the Lithium-Ion battery. These batteries have a higher energy density than previous generations, meaning they can store more power in a smaller, lighter package. This has led to longer battery run times, more consistent power output, and a reduced rate of power loss when not in use. Additionally, lithium batteries are more environmentally friendly than older battery types, further enhancing the appeal of eco-friendly tools.
Several key factors have aligned in recent years to make this shift not only possible but inevitable. Lithium-Ion batteries have been in development for decades, but recent advancements in material science, manufacturing techniques, and energy management systems have drastically improved their capabilities. One major breakthrough is the significantly higher energy density of Li-Ion batteries compared to older technologies like Nickel-Cadmium (NiCd) and Nickel-Metal Hydride (NiMH). This allows for more power to be stored in smaller, lighter cells, which has revolutionized the design and functionality of cordless tools. Users no longer need to sacrifice power or runtime for portability. In fact, modern Li-Ion batteries provide extended runtimes that rival or even surpass the fuel capacity of many gas-powered tools, enabling professionals to work longer without interruption.
The timing of this revolution is also linked to the rise of advanced battery management systems (BMS) that now accompany Li-Ion batteries. These smart systems are engineered to communicate directly with the tool, adjusting power output to match the tool's requirements and preventing issues like overloading, overheating, or deep discharge, which were major pain points for earlier battery platforms. By optimizing performance in real time, these BMS innovations have significantly improved battery lifespan, safety, and overall tool efficiency.
With a growing global focus on sustainability, Lithium-Ion batteries are less harmful to the environment than their predecessors, producing fewer toxic materials and lasting longer, which reduces waste. This eco-friendly advantage, combined with the push for reducing reliance on fossil fuels, has driven both consumer and industrial demand for cleaner, battery-powered alternatives. The development of more efficient recycling methods for Li-Ion batteries further strengthens their position as a future-proof solution.
Performance Considerations: What’s Right for You?
When looking for commercial grade power, gas-powered tools used to be the obvious choice. Today, with the performance of battery tools matching or surpassing gas-powered options, the decision becomes more about which tool suits your specific needs. The freedom to move without being restricted by cords or the need to carry fuel is a significant advantage, especially in industries where mobility can dramatically impact productivity.
That said, there are certain conditions where gas-powered tools might still be preferable. In extremely cold weather, battery run time can be reduced. But for most daily or regular use cases, battery tools have become the go-to option, offering unmatched convenience and performance.
Regulatory and Environmental Considerations
In certain areas, regulatory changes are driving the shift toward battery-powered tools. California has completely banned gas-powered tools with other states likely to follow. Additionally, local noise ordinances in many regions now restrict the use of loud, gas-powered outdoor equipment. In such areas, battery tools are not just a preferred option—they're a legal necessity.
Overcoming Challenges in Outdoor and Remote Work
Portable Power Stations
A primary concern for professionals working outdoors or in remote locations has been the availability of power. This limitation often made gas-powered tools the default choice. However, advances in battery technology have effectively addressed these concerns. Modern battery tools offer significantly longer battery run times, allowing for a full day's work without the need for recharging.
Moreover, the development of portable power stations has revolutionized how professionals approach remote work. This innovation ensures that even in the most remote locations, power is always within reach, making battery tools a viable option for outdoor and remote work environments.
Industries in Transition: From Gas to Battery Power
Several industries that have traditionally relied on gas-powered tools are now transitioning to battery-powered alternatives, thanks to the improved performance and convenience of modern battery tools.
Construction and Landscaping

In construction and landscaping, the perception has long been that certain tools, such as compressors, saws, lawn mowers, chain saws, and weed wackers, must be gas-powered to deliver the necessary performance. However, this perception is increasingly outdated. For instance, Milwaukee's M18 FUEL chainsaw has been proven to deliver more power than a 40cc gas chainsaw, challenging the conventional wisdom in the landscaping industry.
Similarly, battery-powered compressors and saws from Makita and DeWalt are now available, offering the same level of performance as their gas-powered counterparts but with the added benefits of being more portable and eco-friendly. These tools not only reduce noise and emissions but also require less maintenance, making them a more cost-effective and environmentally responsible choice.
Plumbing
Plumbing Tools
The plumbing industry has also been slower to adopt battery tools, largely due to concerns about power and battery run time. However, the latest generation of battery-powered plumbing tools offer the power and durability required for heavy-duty tasks. Tools like cordless pipe cutters, press tools, and drain cleaning machines are now widely used for heavy-duty applications. These battery-powered alternatives deliver the torque and reliability required to cut through thick pipes, crimp fittings, and clear clogged drains with ease. For instance, battery-powered pipe threading and cutting tools offer the same precision and durability as their corded or gas-powered counterparts, but with the added benefits of portability and reduced noise. Press tools, which are essential for creating secure, leak-proof connections, now come in battery-powered versions that save time and effort on the job.
Additionally, battery-operated drain cleaning machines are increasingly favored for their quiet operation and reduced maintenance compared to traditional gas-powered models. These tools are not only comparable in performance to gas-powered options but also offer reduced noise levels, lower maintenance requirements, and greater ease of use, making them an increasingly popular choice among professionals.
Facility Maintenance and Warehouse

In the facility maintenance and warehouse industry, the adoption of battery-powered tools has surged as new technology meets the demands of this fast-paced, heavy-duty environment. Key tools such as cordless impact wrenches, drills, saws, and grinders have become indispensable for facility maintenance teams tasked with everything from equipment repair to structural adjustments. Battery-powered impact wrenches, for example, deliver the high torque needed to loosen or tighten bolts on machinery and racking systems, while cordless drills are used for assembling shelving units or performing routine repairs. In warehouses, cordless pallet jacks and lift trucks have transformed material handling, providing operators with the freedom to move goods efficiently without the restrictions of power cords. For tasks like cutting or grinding metal components, battery-powered angle grinders offer both the power and flexibility needed for on-the-spot repairs or adjustments. Additionally, floor care tools such as battery-powered sweepers and scrubbers provide an eco-friendly solution for maintaining clean and safe workspaces. With reduced noise, enhanced mobility, and fewer maintenance requirements, these battery-powered tools are reshaping how facility maintenance and warehouse operations are managed, leading to greater productivity and ease of use.
CONSIDERATIONS
Cost Considerations
While the upfront cost of battery tools is typically higher due to the expense of electronic components and lithium batteries, the total cost of ownership often proves to be lower. Battery tools require less maintenance and have lower operating costs (no fuel required). Plus, lithium batteries are becoming more affordable as technology improves.
Over time, the reduced energy costs and decreased need for replacements make battery tools a cost-effective choice. In many cases, professionals can recoup their initial investment within a few years, making battery-powered tools an economically sound decision for the long term.
Environmental Impact
The environmental benefits of battery tools are another significant factor driving their adoption. Gas-powered tools contribute to air and noise pollution as well as the depletion of fossil fuels. In contrast, battery tools produce zero emissions during operation and are generally quieter, reducing noise pollution in both residential and commercial areas.
As the energy grid continues to shift toward renewable sources, the carbon footprint of charging lithium batteries will further decrease, making battery tools not only practical for today but also a sustainable choice for the future. The adoption of eco-friendly tools is not just a trend—it's a responsible choice that aligns with global efforts to reduce environmental impact.
The evolution of battery tools has reached a point where they are no longer seen as secondary options to gas-powered or tethered tools. Global Industrial is the source for industrial equipment, providing the latest cutting edge technologies to power your business. In addition to carrying the top national brands, Global Industrial features the best battery-powered equipment such as our new portable power system, tugger, and sweeper.
Additional Considerations
Safety is another big issue when considering making the switch to battery-powered tools. Imagine it - no more dealing with hazards associated with power cords, such as tripping or accidental disconnection. Without the need for fuel or power cords, the risk of fire or electrical shock is significantly reduced, making battery tools a safer option in confined spaces or hazardous conditions. Additionally, battery technology has advanced to include features like thermal management and overload protection, which prevent overheating and ensure consistent, safe performance during extended use.
Noise reduction is another key consideration. Battery-powered tools tend to operate more quietly than their gas-powered or pneumatic counterparts. This is particularly beneficial in environments where noise pollution can disrupt workflow or pose a safety risk, such as in indoor facilities or residential areas. This lower noise level not only protects workers' hearing but also promotes a more comfortable work atmosphere. Moreover, reduced vibration in many battery-powered tools contributes to operator comfort and reduces long-term strain. These factors combine to make battery-powered tools a safer, more user-friendly option for a wide range of industries, further driving their adoption in professional settings.
For more on the latest battery powered technology, please visit GlobalIndustrial.com and be sure to check out our New Products, Workspaces, and Seasonal Solutions
The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.