Vostermans Mechanical Thermostat For Fan Or Heater TT15WDCAM1A Single Pole

Rollover image to zoom in

Click image to enlarge

See all 40 items in product family

Vostermans Mechanical Thermostat For Fan Or Heater TT15WDCAM1A Single Pole

Item #: WB245823

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 45.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
THERMOSTATS AND TRANSFORMERS
Mechanical Thermostat for Fan or Heater Combination Control up to 2 devices. Can be used to operate fans, heaters, curtains on livestock buildings or any other electrical device needing automatic control. Water and dust resistant high impact plastic housing. Fire resistant for trouble free operation. Operating temperature range of 32 to 104°F. Operates 120V or 240V. 10 Amp maximum load. CSA approved.

Documents are in PDF format

Product Specifications

    • BRANDMultifan
    • WIDTH INCHES4
    • DEPTH INCHES2-1/2
    • HEIGHT INCHES5
    • WEIGHT LBS1
    • CONSTRUCTIONImpact & Fire Resistant Poly Box
    • TEMPERATURE CONTROL RANGE °F32 to 104
    • VOLTAGE240 / 120
    • STAGES1H
    • DESCRIPTIONMechanical Thermostat
    • TYPESingle Pole
    • LIMITED WARRANTY YEARS1
    • MANUFACTURER'S PART NUMBERTT15WDCAM1A
    • MODEL245823
Have A Question About This Product?
1 Question | 1 | Answer

Avg. Customer Rating: (17 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating
Sort by: 

17 Results

thermostat

Your review: This thermostat replaced one that had gone out in a heater used in a green house. It arrived promptly, was easily installed and has worked efficiently every since

Pros: Efficient, easy install, good quality, good value.

Is this review helpful?

Thermostat for Fans

Your review: These units insure fans only run when needed. I've had no problems with them.

Pros: Fair pricing. They save energy. Dependable.

Cons: No issues.

Is this review helpful?

Thermostat

Your review: This was just what I needed and was very easy to install and works very good.

Is this review helpful?

thermostat control-vostermans

Your review: Good quality product. works well in adverse enviornments

Is this review helpful?

Works great

Your review: Using this to regulate the fan in our greenhouse, works great. Just what we needed. Could not find it in our town, was glad to find this one.

Pros: none

Is this review helpful?

Thermostat Controler

Your review: Working well, sensitivity is not the best temp range for on/off is between 2 to 4 degrees, but its doing the job

Pros: Price was good - construction is good

Cons: Wiring diagram was really POOR- and also operations are reversed of the drawings- once I figured it out it- all is fine

Is this review helpful?

Mechanical thermostat

Your review: So far so good.

Pros: Easy install.

Cons: None so far

Is this review helpful?

Great choice for our use

Your review: Great choice for a thermostat. No electronic stuff to mess up and no batteries needed...old school is sometimes the best.

Pros: No batteries Ease of installation

Cons: not exactly "pretty" but it is very functional. It controls the attic/exhaust fan in our house and could care less what it looks like as it's in the attic.

Is this review helpful?

Does What It Says

Your review: Keeps our exhaust fan on and off when we need it.

Pros: Keeps us from having to turn fan on and off.

Cons: Cant think of any.

Is this review helpful?

thermostat

Your review: Works great I put a thermometer next to it and it is quite close. Fan goes on at 85 degrees

Pros: Was very easy to install

Cons: none

Is this review helpful?

Mechanical Thermostat

Your review: Just installed about a week ago. Seems to work as advertised. Time will tell but I expect no problems. It is Manual!

Is this review helpful?

Thermostat

Pros: Works great

Is this review helpful?

Mechanical Thermostat Review

Your review: I was very impressed with the quality and price of the Vostermans Mechanical Thermostat, Model TT15WDCAM1A. For the do-it-yourself homeowner like myself, I did find the installation instructions hard to follow because the wiring diagram was not clear as to how to connect the fan to the thermostat. I called Global and in turn was contacted by a Vosterman technician who set me straight on the connections. I would recommend that the instructions be re-written to make installation connections clear for those who are not electricians by trade or experience. Overall, I am pleased with my purchase and the thermostat works like a charm so far.

Is this review helpful?

Vostermans Mechanical Thermostat TT15WDCAM1A

Your review: I just finished installing an exhaust fan in my garage to keep it from heating up on very hot days (sometimes over 115 degrees). I installed the subject thermostat to the fan so it would start exhausting at a much lower temp. The thermostat works perfectly, and I'm delighted with it. I was not, however, happy with the installation instructions that came with the thermostat, nor the instructions which I downloaded from your website. Neither of them was properly labeled to be able to easily identify the hot black wire and the white neutral wire. The instructions from your website were the best, but could have been much better if the wire going from the "2" to the what looks like a battery (which I later learned from Steve in response to my emailed question, was supposed to be an icon for one of your fans) was labeled as black, and if the fan icon was also labeled so that you can tell it does not represent a battery.

Is this review helpful?

Mechanical T-Stat

Your review: I have this T-Stat connected in series with an on-off switch, and a 16" attic fan. I checked the set point vs. actual temp. and it was "right on"..... It's been hot here the past couple weeks, and the T-stat/fan are doing there jobs...no problem

Is this review helpful?

Thermo-tastic

Your review: This unit was very easy to install and setup. We used it to run two through the wall fans and it works like a champ!

Is this review helpful?

Thermal switch

Your review: Works perfect.

Is this review helpful?

Sort by: 

17 Results

There are 17 questions and 1 answers for this product.

Sort by: 

17 Results

What the operating differential temperatures? In other words if the stat is set for 70 at what rising temp would the fan shut down. And at what lowering temperature would the fan start again?

Question Asked By: Al , January 16, 2015

+ View 1 Answer

Answer This Question

Sort by: 

17 Results

Customers Who Viewed This Also Viewed