GreenWorks® 27022  14" 10 Amp Corded Dethatcher

Rollover image to zoom in

Click image to enlarge

GreenWorks® 27022 14" 10 Amp Corded Dethatcher

Item #: WBB779616

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 128.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
GreenWorks Electric Dethatcher

Features:
  • 10 A motor
  • 14" Dethatching path
  • BONUS: includes full set of replacement tines
  • Stainless steel tines stay sharp longer for reliable performance
  • Ergonomic, padded grip and bale switch for added comfort and control
  • Cord lock holds extension cord securely in place
  • Includes: Dethatcher, 18 replacement tine assemblies (36 total tines)
  • 3-position tine depth adjustment provides greater control by removing matted layers to promote continued healthy lawn growth
  • Weight: 25.92lbs / 11.8kgs

Product Specifications

    • AMPS10
    • VOLTAGE--
    • MANUFACTURERS PART NUMBER27022
    • MANUFACTURER LIMITED WARRANTY YEARS4
    • WEIGHT LBS25.92
    • CALIFORNIA EMISSION COMPLIANTYes
    • START TYPEBale Switch
    • ENGINE/MOTOR TYPEElectric
    • CORDLESS OR CORDEDCorded
    • TYPEDethatcher
    • BATTERIES REQUIRED0
    • BRANDGreenWorks®

Avg. Customer Rating: (16 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Nice product

The Greenworks dethatcher did a very nice job dethatching our lawn as well as my sons lawn. Great for average size lawns. I would recommend it so I gave it a 5 star

See more favorable reviews

The most critical review

  • Customer Rating
Sort by: 
1 ...

16 Results

Nice product

Your review: The Greenworks dethatcher did a very nice job dethatching our lawn as well as my sons lawn. Great for average size lawns. I would recommend it so I gave it a 5 star

Is this review helpful?

Excellent home lawn tool

Your review: This is an excellent device that folds-up nicely but I would like to know how to purchase additional sets of tines

Pros: Easy to use, best to lightly dampen lawn to keep dust down. Folds up and stores easily.

Cons: No Cons, just need to know how to purchase additional sets of tines.

Is this review helpful?

Mr.

Your review: Great light duty unit.

Pros: Comes with extra thatcher spring.

Is this review helpful?

GreenWorks 27022 Electric Dethatcher

Your review: This electric dethatcher worked super. I had some dead grass in the back yard and cut it down to 2". I couldn't believe how much dead grass came up.

Cons: I would highly recommend this dethatcher to everyone. It sure beats trying to dethatch the lawn with a rake.

Is this review helpful?

5 stars

Your review: The only trouble you will get tired of picking up the dead grass. It works great !!!

Pros: It is light and works very well. The price is great and no gas to worry about.

Cons: Nothing .

Is this review helpful?

GreenWorks27022 electric Dethatcher

Your review: This machine paid for itself in the first use. It's a little flimsy but does a terrific job. I did a fifty by fifty lawn in less then an hour where it would have taken many hours and blisters if I had to do it by hand. For me, it is a great little machine. Not too heavy and easy to use. I highly recommend it for a not to large lawn.

Pros: Does exactly what is claimed. Light and easy to put together with a single screw driver. No gas or oil or pull starting. Just push the button and your off.

Cons: The only con is you have to drag around an extension cord.

Is this review helpful?

Performs as expected

Your review: I read the reviews by others before I purchased. It performs just as I expected.

Pros: The price was right.

Cons: no cons

Is this review helpful?

Great little machine

Your review: I read other reviews on Amazon.com and other sites about this dethatcher and they sounded great. After hearing my best friend talking about busting his back while doing his dethatching by rake, and seeing his awful blisters. I looked this up and decided to buy it. Used it for the first time today and it was amazing. Of course this is intended for small lawns. My lawn is less than half an acre. It basically propels itself along, and is even quieter than a vacuum cleaner. I did my yard and raked up the clippings in less that 2 hours. Great purchase, all my friends will be using it

Pros: Light weight, Propels itself, Fast, Easy clean up, Does the job in one pass

Cons: Need plenty of long extension cords that you will be dodging, Must wait til ground is completely dry since it is electric,

Is this review helpful?

This is great

Your review: easy to use, this will help my grass be the best in town, I love it

Pros: all good

Cons: none

Is this review helpful?

Greenworks Dethatcher

Your review: I attached the handle very easily. But read the directions all the way through first. There is an electrical cord holder that needs to be installed on the middle bar before the handle is attached to the machine.

Pros: Works great, fast and amazing.

Cons: Back wheels should be larger so you can roll across driveways, ect. without damaging thatcher springs

Is this review helpful?

Excellent

Your review: This works perfectly for thatching and the service you provided was excellent. I will know more when I use it in the future as to the durability of the machine.

Pros: Easy to use, quiet, lightweight.

Cons: None I can think of

Is this review helpful?

Greenworks Dethatcher

Your review: Easy to assemble and very reasonably priced.

Pros: Light and easy to use!

Cons: None

Is this review helpful?

Dethatcher

Your review: Make sure it is set on the highest setting before you start, I didn’t try, but I suspect the lower settings would dig things up, considering how well the highest setting worked.

Pros: Worked well.

Cons: It took a couple of tries to get the line cord install to match the picture.

Is this review helpful?

GreenWorks Electric Dethatcher

Your review: Received our order promptly for the Electric Dethatcher and in good condition.

Pros: Works good.

Cons: None

Is this review helpful?

love it

Your review: I have a 53x54 ft back yard, I tried it with the rake last year,this year I got smart and purchased this machine.It does a good job very quickly. I can see why this machine was sold out,but you got it to me a month before estimated time and it was definitely worth the wait.

Pros: Easy to assemble, runs smoothly. very nice that extra tines are supplied in case of breakage.

Cons: could make the cord clip a bit wider I used a 14 gauge extension and had to really bend it to get it in.

Is this review helpful?

A salesman in itself!

Your review: Simply an amazing machine! Can not be beat for the price. Prior to this purchase I had a pull behind dethatcher for my tractor. It was difficult to get corners and specific locations as my yard has a good deal of landscaping. The pull behind also had a tendency to tear up a good amount of green grass too. Within 15 minutes of starting I was asked by a motorist driving by where I purchased the Greenworks dethatcher. By the end of the day there were six people asking about the little machine and all loving the results. In my front yard alone I filled 4 yard bags with dead grass and only dead grass. There was no green grass removed. That in itself amazed me. In one day I did two yards front and back and one yard front using a mower with a catcher to pick up the thatch. I'm sold!

Pros: Easy, lightweight, does not tear up good grass, gets into small areas, works so well it draws attention from passersby

Cons: narrow path, working around extension cords....that's it

Is this review helpful?

Sort by: 
1 ...

16 Results

Be the First to Ask a Question!