General Wire KR-D-WC Kinetic Water Ram Manual Drain Cleaner W/Case

Rollover image to zoom in

Click image to enlarge

General Wire KR-D-WC Kinetic Water Ram Manual Drain Cleaner W/Case

Item #: WBB213988

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 414.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
General Wire Kinetic Ram Pipe Cleaner w/6" Rubber Cone, Four Expansion Plugs, Closet Attachment, Check Valve, Water Supply Hoses, Universal Faucet Adapter & Case

Here's a compact, lightweight tool for quickly opening clogged sinks, toilets, and tubs. It handles rust, grease, sediment, and scale in lines up through 4" in diameter.The Kinetic Water Ram uses a burst of compressed air that drives a shock wave (kinetic energy) through water to break up stoppage. It's particularly useful when the stoppage is on the far side of a drum trap or series of tight bends, since the shock wave can travel around bends without losing its force. The Kinetic Water Ram has a self-contained pump and pressure gauge, so you can hit the stoppage with just the rightamount of force. You get instant impact with no build-up of pressure in the plumbing system. The force is transmitted through water, so it's not affected by stacks or vents. The included toilet attachment (KR-CA) screws onto the front of the Kinetic water Ram and enables you to position the cone in the bowl to get a tighter seal. As a result, you can strike the blockage with greater impact and no splash back. Store the Kinetic Water Ram and its accessories in the carrying case.

Click for Operating Instructions
Click for Parts List and Schematic Drawings

Product Specifications

    • LENGTH INCHES21
    • WIDTH INCHES4-1/4
    • HEIGHT INCHES6-1/2
    • CONSTRUCTIONSteel
    • BRANDGeneral Wire
    • DESCRIPTION4" & 6" Cones, 5 Plugs, 4 Extension Plugs, Check Valve, Supply Hose, Adapter
    • MAX CABLE LENGTH FEET21
    • PACKAGE QUANTITY1
    • WEIGHT LBS9
    • SERIESKinetic Water Ram
    • INCLUDES4 & 6 Cones, 5 Plugs, 4 Extension Plugs, Check Valve, Supply Hose, Adapter, & Ca
    • FOR USE WITH PIPE SIZE INCHES1-1/4 to 4
    • MANUFACTURERS PART NUMBERKR-D-WC

Avg. Customer Rating: (6 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Great

After using a cable machine and not being able to reach the plug at 75 feet. I bought the water ram. Pumped it up to 30 psi pulled the trigger and bam The plug released. Wow took all of 15 minutes. The plug was in a University's 3 inch pool shower line. Super happy with the results.

See more favorable reviews

The most critical review

  • Customer Rating

Great

After using a cable machine and not being able to reach the plug at 75 feet. I bought the water ram. Pumped it up to 30 psi pulled the trigger and bam The plug released. Wow took all of 15 minutes. The plug was in a University's 3 inch pool shower line. Super happy with the results.

See more critical reviews

Sort by: 
1 ...

6 Results

Great

Your review: After using a cable machine and not being able to reach the plug at 75 feet. I bought the water ram. Pumped it up to 30 psi pulled the trigger and bam The plug released. Wow took all of 15 minutes. The plug was in a University's 3 inch pool shower line. Super happy with the results.

Is this review helpful?

Works Great

Your review: Used in our cafeteria sink and also men's room sink. Worked perfect both times. No mess at all.

Is this review helpful?

The ultimate plunger

Your review: I spotted my engineer crawling into the wall between the men's and women's restrooms to auger out the common lateral for both sets of toilets. When asked if he had tried our new kinetic ram, he had not. So he waited inside the wall, perched on the plumbing while I got our new tool. Instructions said to start at 10psi, I started at 15. I half expected water to jump out of adjacent plugged toilets when I actuated the handled. It seemed like nothing happened. As I started to pressurized the tool again, all of the toilets started to flush. Later, my engineer tried it on a long-standing slow-draining sink with the same result. This sink had been augered numerous times over the past few years. We are sold. What a beautiful plumbing tool.

Is this review helpful?

Very Nice

Your review: Professional grade. High quality. High price. Nobody else seems to be making a similar product anymore.

Is this review helpful?

air ram

Your review: there is nothing to be said about it it just works you have to learn what uses it is good for but there is no other tool for what it does

Is this review helpful?

ANSWER IN A BOX

Your review: I have used one of these marvelous tools years ago and sold it due to illness. I recently recovered enough to work part time as maintenance again for a property owner and this tool and it's accessories is the answer to so many issues that come up on rental's! The feeling of saving money and opening drains so easily with this wonder machine is incredible. I recommend anyone with any properties at all to buy it and the return will pay for itself in no time! Its a no brainer, for sure. Thanks for this opportunity to express my love of the whole kit!

Is this review helpful?

Sort by: 
1 ...

6 Results

Be the First to Ask a Question!