Steel Portable Barricade Gate With Casters

Rollover image to zoom in

Click image to enlarge

See all 3 items in product family

Steel Portable Barricade Gate With Casters

Item #: WB955042

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 146.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Portable Pedestrian Barricade
with Casters

Create a barricade anywhere it's needed in seconds. This portable pedestrian barricade has lightweight aluminum slats with steel ends. Weighs only 46 lbs. and measures 40"H when folded. Expands from 16" to 141"L. Yellow and black slats. Includes 4 swivel casters for mobility. The distance from the ground to the bottom of the gate when full opened is 13.39"; while fully closed is 8.27". 11-1/4" in between casters.

Product Specifications

    • LENGTH INCHES16 to 141
    • HEIGHT INCHES40
    • COLOR FINISHYellow/Black
    • BRANDGlobal Industrial™
    • DESCRIPTIONWith Connection Hinge
    • ASSEMBLYAssembled
    • CONSTRUCTIONSteel
    • EXPANDED LENGTH INCHES141
    • WEIGHT LBS46
    • EXPANDED HEIGHT INCHES40
    • MODEL955042
    • TYPEWith Casters
Have A Question About This Product?
4 Question | 4 | Answer

Avg. Customer Rating: (28 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating
Sort by: 
1 2 ...

28 Results

collaspsable barricades

Your review: good product. Handy for the need we bought them for.

Pros: easily moved and space saving when not in use

Cons: Not all the bars for holding them collapsed were bolted on.

Is this review helpful?

Barricade gate

Your review: I have ordered 12 of these gates and they work great for our needs

Pros: Very easy to use

Cons: none

Is this review helpful?

Great for Security Usage

Your review: Began using these barricades instead of stanchions to block off secure areas. Have made an immediate noticeable difference as soon as they were put into use. Fantastic way to secure large, open areas.

Pros: They are more noticeable. Cannot be easily opened like with the stanchions we were previously using. Very easy to set up and store on a daily basis.

Cons: They are heavy, but having wheels helps. Are still looking for a way to secure them at each end to stop unauthorized access.

Is this review helpful?

Safe security

Your review: We use ours to block off areas for forklift use. Easy use and easy storage.

Is this review helpful?

Visual deterrent

Your review: This is our second expando gate. Convenient, portable, store-able. Yes, they will flop over at full extension if not pinned to wall but it is not a true security gate anyway. What it does is remove excuses for being in the wrong area when Murphy strikes.

Is this review helpful?

Excellent Safety Product

Your review: To meet code requirements, a section of one of our buildings needed to be sectioned off, but we still needed access for facilities. This unit works great and locks in with other users to provide an expandable solution.

Is this review helpful?

steel portable Barricade Gate w/ Casters

Your review: work exelent that is exacly what I was looking for . thank you.

Is this review helpful?

does what it should

Your review: PUrchased this to identify where public should not access beyond point while employees passing constantly throughout the day. The wheels make it easy for employees to move to pass through but replace. Customers have not "wandered" like before!! Problem solved!

Pros: Durable. easy to move and position in place hard to not notice

Cons: none so far

Is this review helpful?

Great product

Your review: Fastest shipping ever and no damage to a heavy parcel quick setup.....I would buy again....

Is this review helpful?

Nice Gates

Your review: These gates are very economical and work great for blocking our docks.

Pros: Very easy to assemble

Cons: Took a long time for delivery

Is this review helpful?

Strong and Portable

Your review: This was the perfect item for barricading an area we have trouble with illegal parking. They fold up relatively compact which help with limited storage space. We used large zip-ties ti temporarily bind them and that kept folks from separating the sections. I recommend this to anyone needing a portable barricade system.

Pros: Relatively inexpensive, portable, small storage footprint, easy to see, wheel casters.

Cons: A few minor parts were missing with the hardware, but nothing we couldn't work around.

Is this review helpful?

Steel Portable Gate

Your review: Makes the job much easier to move around with casters

Pros: works great for us

Cons: none

Is this review helpful?

Well built, could use a couple of changes

Your review: i work at a manufacturing company with a very active employee group, and one of our favorite things to do at break time is Ping-pong. the freight crew was increasingly frustrated by people running after ping pong balls while they were unloading containers. these gates make a solid line of safety around the work area and everybody is happier.

Pros: Well built and stable. nice casters that roll well on concrete. the units train together to make longer barricades. there is a lock to hold them closed.

Cons: I wish there werelocks to hold the barriers open. They tend to shorten up and try to close after a while. They are also difficult to hook together to make a longer barrier. You have to pick one up completely and drop its pin into the socket of the next one. i don't want to be the person to file an incident report regarding a back injury sustained while setting up a safety barricade. A pin on a chain and a socket with holes would be a better way to hook them together.

Is this review helpful?

Barricades

Your review: Just what I was looking for.

Pros: Very good value

Cons: A special THIN wrench is needed to tighten the casters to the frame. None was included with the unit. I had to use a thin 'vise grip' that I happened to have but even then I was only able to grab onto the outer edge of the bearing race and not the hex part of the spindle. This caused the race to slip in relation to the hex part once the threads tightened. I hope this will not cause the joint to loosen up prematurely.

Is this review helpful?

unsafe

Your review: When the gate is fully extended it bows in the middle and falls over. It is also heavy and has no brakes to hold it on an incline.

Pros: Looks like it would work good.

Cons: Falls over, heavy and has no brakes to hold it in place.

Is this review helpful?

great gate!

Your review: This gate is durable and is exactly what I was looking for to put in front of my business.

Is this review helpful?

Portable barricade

Your review: This is an excellent product. Very well constructed. Globals price on the unit is very fair for the quality of the product received.

Is this review helpful?

Nice for the price

Your review: These work pretty well. Assembly was easy. When fully opened, they did tend to close themselves, but tightening the nut/bolt on the one end of the scissor took care of that problem.

Is this review helpful?

Portable Steel Barricade Gate

Your review: This steel portable barricade gate w/casters is just what I was looking for to stretch across my driveway. I live on a four lane road and a couple of times someone drove into my driveway and broke those gates. Well this one may be the first and last gate they hit.

Is this review helpful?

Good for Pedestrian traffic

Your review: Overall this gate does a good job for my needs. It is used to block a bay door that is used primarily for ventilation. I had to add chains so that I could secure this to the wall to prevent people from pushing it aside. Otherwise I'm satisfired with the product.

Is this review helpful?

Great quality for price.

Your review: When I saw these in the catalog I thought to my self this is perfect for some needs in my facility. When I looked at the price I thought it was going to be a poor quality. After assembling and using for the last couple weeks. I should have never second guessed myself. I currently use it as a barricade when we have our orchestra pit open in our theater. It is functional and professional looking as well. Only drawback is that the casters are not locking.

Is this review helpful?

Portable Barricade with casters

Your review: Steel barricade with casters, much easier to use than the plastic barricades. Hooks into other barricades easily to make a wider barricade. Casters make it easy to move around.

Is this review helpful?

Not suitable for extension of more than 4-5 feet

Your review: I purchased these units since the description stated that it could expand to 11ft and the pictures showed a fully extended unit, but when I assembled the product, I found that the unit would lose stability when extended more than 4-5 feet since the casters do not lock and the bases are not wide enough to support the weight of the unit when fully expanded. The gate begins to bow and at 45 lbs, structurally the design is not capable of supporting the instability and will result in the unit either toppling over or the bases and wheels turning inward to compensate for the in-balance. I would not recommend purchasing this unless you only need to section off a small aisle or if you can either attach the base to something stable or use a weighted object (sandbags) to prevent the casters from moving although this defeats the purpose of a portable barricade.

Is this review helpful?

Best Products.....With Good Price

Your review: Best Products...Supper fast shipping...A++++ service....Must buy ...Thanks

Is this review helpful?

Sort by: 
1 2 ...

28 Results

There are 28 questions and 4 answers for this product.

Sort by: 
1 2 ...  

28 Results

Are the Casters removable?

Question Asked By: SHANNON , February 01, 2018

+ View 1 Answer

Answer This Question

Does this gate meet OSHA regulations for fall protection at a shipping dock?

Question Asked By: Stan , Strongsville, OH , August 25, 2017

+ View 1 Answer

Answer This Question

Is this product for indoor / outdoor ?

Question Asked By: Prashant Karnik , New Jersey , August 10, 2017

+ View 1 Answer

Answer This Question

Have this Barricade something to lock the casters? Or how could we ensure they never retract or leave on the position we want. Thanks

Question Asked By: Juan Carlos , El Paso, Tx , February 14, 2017

+ View 1 Answer

Answer This Question

Sort by: 
1 2 ...  

28 Results