Universal Tool UT8708, Right Angle Pencil Grinder, 70000 RPM, Rear Exhaust, 0.25 HP
See all 59 items in product family

Universal Tool UT8708, Right Angle Pencil Grinder, 70000 RPM, Rear Exhaust, 0.25 HP

Item #: WBB231423

Sold By: globalindustrial.com

Usually ships in 2 to 5 days Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $189.00 Save up to 5%
Price: $ 178.95
Product Information
Customer Review
Product Q&A
Accessories
Right Angle Pencil Grinder

  • Roll throttle & small diameter grip for constant speed & operator control
  • Supplied complete with coaxial hose assembly
  • Rear exhaust keeps work area clean from cuttings
  • Gearless design reduces maintence costs
  • 70,000 RPM for high speed, precision work
  • Best for: Precision grinding in mold and die maintence

Product Specifications

    • LENGTH INCHES5.9
    • BRANDUniversal Tool
    • DESCRIPTIONRight Angle Pencil Grinder
    • HORSE POWER.25
    • MANUFACTURERS PART NUMBERUT8708
    • COLLET SIZE1/8"
    • RPM70000
    • PRESSURE90 psi-6.2 bar
    • EXHAUSTRear
    • HOSE SIZE I.D1/4
    • AIR INLET NPT1/4
    • TOOL TYPEGrinders
    • MAX WHEEL DIAMETER1/8"
    • SPINDLE SIZE--
    • GUARD TYPE--

Avg. Customer Rating: (5 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Pencil Grinder

Excellent product. Works exactly as expected and as product description. I am very pleased with the grinder.

See more favorable reviews

The most critical review

  • Customer Rating

Pencil Grinder Blues

Bought the pencil grinder and seemed to be fine, but I had heard that the design of the collet was not good. The collet broke during what was a normal use for the tool. I called customer service and was instructed to call a service center in KC. They told me they had to order the part from the manufacturer in FL. for $14.10 each. Not at all what I expected. I would like to return it for a full refund...and find one with a better designed collet.

See more critical reviews

Sort by: 
1 ...

5 Results

Pencil Grinder

Your review: Excellent product. Works exactly as expected and as product description. I am very pleased with the grinder.

Is this review helpful?

Right Angle Pencil Grinder

Your review: fast shipping I only used it twice so far with a 3/4" disc, seems to run smooth and accurate. I would buy this again !

Is this review helpful?

Pencil Grinder Blues

Your review: Bought the pencil grinder and seemed to be fine, but I had heard that the design of the collet was not good. The collet broke during what was a normal use for the tool. I called customer service and was instructed to call a service center in KC. They told me they had to order the part from the manufacturer in FL. for $14.10 each. Not at all what I expected. I would like to return it for a full refund...and find one with a better designed collet.

Is this review helpful?

Angle Pencil Grinder

Your review: Product is what I expected. Seems to be a very well made grinder. It compares well to the ones offered by the tool trucks that service where I work. The price is better even with shipping and handling. I have recommended it to several other cabinet makers that have borrowed it and liked it. The only thing about it is that other grinders have a similar collet which I have been told can break rather easily, but at this time I have seen no problem with it. THANKS...

Is this review helpful?

right angle pencil grinder

Your review: Great product no problems

Is this review helpful?

Sort by: 
1 ...

5 Results

Be the First to Ask a Question!