Canopies, carports, and utility tents create versatile outdoor spaces for events and trade shows. Utility tents are constructed from heavy duty materials and are easy to assemble and break down. Canopies can act as temporary shelters to provide shade from the sun and protect from weather conditions such as rain.
Storage Tents
(110 Products)
+ View All
Carports
(26 Products)
Carport Accessories
Double Carport
Single Carports
+ View All
Canopies
(98 Products)
Commercial Canopies
Portable Canopies
Heavy Duty Canopies
Long Legs End Panels
And more......
+ View All
Canopy Stakes & Anchors
(24 Products)
Anchors & Mounting Feet
Mounting Stakes
+ View All
Utility & Work Tents
(14 Products)
Straight Leg Pop-Up Canopies
Tent Sidewalls
Straight Leg Pop-Up Canopies with Sidewalls
+ View All
Canopies, Carports & Utility Tents for Outdoor Shelter and Storage
Canopies, carports, and utility tents provide flexible outdoor space for shade, weather protection, storage, work areas, and temporary operations. Depending on the design, they can shelter vehicles and equipment, provide covered space for events and outdoor activities, or create temporary work and storage areas. Options include portable canopies, commercial canopies, storage tents, carports, and utility and work tents.
How to Choose a Canopy, Carport, or Utility Tent
Choosing the right outdoor shelter depends on how it will be used, the amount of space needed, how often it will be assembled or moved, and the weather conditions it will encounter. Consider these factors before selecting a model:
Type: Choose a canopy for shade and general outdoor coverage, a carport for vehicles and larger equipment, or a storage or utility tent when enclosed or partially enclosed space is needed for storage or work activities.
Size: Consider the footprint of the area that needs to be covered as well as the height and dimensions of vehicles, equipment, or other items that will be placed underneath.
Material: Frame and cover materials affect durability, weight, maintenance, and weather performance. Review the product specifications to select materials suited to the intended application.
Weather protection: Consider exposure to sun, rain, wind, snow, and changing temperatures. The level of protection varies by product, so review the manufacturer's specifications before installation and use.
Anchoring and stability: Proper anchoring helps keep outdoor structures stable during use. Select compatible stakes, anchors, mounting feet, or other accessories based on the structure and installation surface.
Sidewalls and enclosure: Sidewalls can provide additional protection from weather, wind, and surrounding activity. They can also help create a more defined work, storage, or event area.
Portability and setup: If the structure will be moved or assembled frequently, consider its setup method, portability, storage requirements, and the number of people needed for assembly.
Canopies vs. Carports vs. Utility & Storage Tents
Different outdoor shelters are designed for different applications. Use the table below to help determine which type is appropriate for your needs.
Type
Primary Use
Common Applications
Canopies
Provide temporary shade and covered outdoor space
Events, outdoor work areas, entrances, gatherings, and temporary shelter
Carports
Cover and protect vehicles or larger equipment
Cars, trucks, trailers, equipment, loading areas, and outdoor parking
Storage Tents
Create covered or enclosed outdoor storage space
Vehicles, equipment, materials, seasonal items, and inventory
Utility & Work Tents
Provide temporary covered workspace or work areas
Maintenance, construction, events, service work, and temporary operations
Common Uses for Canopies, Carports & Utility Tents
Outdoor shelters can provide additional covered space for commercial, industrial, facility, maintenance, and event applications, including:
Protecting vehicles, trailers, and equipment from sun and weather
Creating temporary outdoor work areas
Providing covered space for maintenance and service activities
Storing equipment, materials, and supplies
Providing shade for employees, visitors, or event attendees
Creating temporary areas for trade shows, events, and outdoor activities
Covering loading, staging, or service areas
Expanding usable space without constructing a permanent building
Anchoring Outdoor Canopies and Tents
Proper anchoring is important for the stability of canopies, carports, and utility tents, particularly in outdoor locations exposed to wind. The appropriate anchoring method depends on the structure, surface, installation location, and manufacturer requirements.
Use compatible stakes, anchors, mounting feet, or other approved accessories and follow the manufacturer's installation instructions. Do not assume that a structure is safe to use in severe weather simply because it is designed for outdoor use. Check the product specifications for applicable weather and wind limitations.
Frequently Asked Questions
Have a Question? Our experts might already have the answers.
What is the difference between a canopy and a carport?
A canopy is generally used to provide temporary shade or covered outdoor space, while a carport is designed primarily to shelter vehicles or larger equipment. Carports typically provide a larger covered area and may have a more substantial frame or structure.
What is a utility tent used for?
Utility tents provide temporary covered space for work, maintenance, service, storage, events, and other outdoor activities. Depending on the design, they may be open, partially enclosed, or equipped with sidewalls for additional protection.
What is a storage tent used for?
Storage tents provide covered outdoor space for vehicles, equipment, materials, supplies, and other items that need protection from outdoor conditions. Made from heavy-duty materials for greater durability, they provide long-lasting outdoor storage without requiring a permanent building.
How do I choose the right size canopy or tent?
Consider the area you need to cover and the dimensions of the people, vehicles, equipment, or materials that will be underneath the structure. Also account for clearance around doors, equipment, and walkways. Review the structure's overall dimensions and usable interior space before selecting a size.
Are outdoor canopies and tents waterproof?
Weather protection varies by product. Some canopies and tents are designed to provide protection from rain, while others are intended primarily for shade or temporary coverage. Check the product specifications for information about water resistance, weather protection, and limitations before use.
Can canopies be used in windy conditions?
Outdoor structures can be affected by wind, and stability depends on the structure, anchoring method, installation surface, and weather conditions. Always follow the manufacturer's anchoring and wind guidelines. Take down or secure temporary structures when conditions exceed their specified limits.
Do canopies and utility tents have sidewalls?
Some models include sidewalls or are compatible with sidewalls that can be purchased separately. Sidewalls can provide additional protection from weather and wind or create a more enclosed work, storage, or event area. Check product specifications for compatible accessories.
How do I anchor a canopy or utility tent?
The correct anchoring method depends on the structure and the surface where it will be installed. Options can include stakes, anchors, mounting feet, or other compatible accessories. Follow the manufacturer's installation instructions and use an anchoring method appropriate for the specific application.
Can a carport be used to store equipment?
Yes. Carports can provide covered space for vehicles, trailers, machinery, equipment, and other large items, provided the size, height, weight, and environmental requirements of the structure are appropriate for the intended use.
What is the difference between a temporary canopy and a storage tent?
A temporary canopy is generally designed to provide open covered space, shade, or temporary shelter. A storage tent typically provides a larger covered area and may include enclosed sides or doors to create a more durable protected space for vehicles, equipment, materials, or supplies.