How to Protect Your Facility From Flooding

Key Takeaways:

 

  • Flooding is one of the most damaging and costly events a commercial or industrial facility can face, and facilities that prepare in advance recover faster, at a lower cost.
  • Because facilities must protect large equipment, inventory, utilities, hazardous materials, and an entire workforce, commercial flood preparedness is typically much more complex than residential flood prep.
  • A complete approach covers three phases: protecting the facility before a flood, acting safely during one, and recovering efficiently afterward.
  • Each step connects to specific equipment, from flood barriers, sandbags, and containment berms to sump pumps, dehumidifiers, wet/dry vacuums, and personal protective equipment.
  • Mold and secondary damage can set in within 24 to 48 hours, making fast, well-equipped recovery just as important as up-front prevention.

 

A flood can bring operations to a standstill in a matter of hours. Whether it comes from a severe storm or an overwhelmed drainage system, flooding can inflict severe damage on the building, its contents, and daily operations while threatening employee safety. The recovery is long and expensive, but the facilities that fare best are the ones that prepared before the water ever arrived.

 

It's also a risk that reaches far beyond obvious flood zones. More than 20% of flood insurance claims come from properties outside high-risk areas, and standard commercial property policies typically don't cover flood damage at all. That combination of broad exposure and limited default coverage is exactly why a deliberate flood plan matters.

 

Unlike residential flood preparation, commercial and industrial facilities must protect complex operations, valuable assets, and the people who work within them. This guide outlines practical steps to help protect your facility, before, during, and after a flood, along with the equipment and supplies that can help keep your operation safer and get it back up and running as quickly as possible. (For severe structural, electrical, or contamination issues, always involve qualified professionals and follow guidance from local emergency officials.)

 

Understand Your Facility's Flood Risk

 

Effective flood preparedness begins with understanding your facility's level of risk. Start by determining whether your facility sits in a flood-prone area using Federal Emergency Management Association (FEMA) flood maps and your local planning or emergency management office. Do not assume you are protected because your facility falls outside a designated high-risk flood zone. Many flood insurance claims originate outside mapped high-risk areas, making flood preparedness a smart investment even for facilities that appear to be at low risk.

 

Next, identify what's most vulnerable inside and around your building, such as critical equipment and machinery, inventory and raw materials, electrical and utility systems, records and IT infrastructure, and any hazardous materials on site. Mapping these assets tells you what to prioritize when a warning comes.

 

Finally, make sure employees understand the types of flood alerts, so they know when to prepare and when to act:

 

  • Flood or Flash Flood Watch — flooding is possible; begin preparations and monitor conditions.
  • Flood or Flash Flood Warning — flooding is occurring or imminent; act immediately and evacuate if directed.

 

Before a Flood: Protecting Your Facility

 

The work you do ahead of a flood determines how much you stand to lose. These are the core preparation steps.

 

Elevate and Protect Equipment, Inventory, and Records

 

Move what you can above expected flood levels:

 

  • Relocate equipment, inventory, and critical records to higher shelving, upper floors, or off-site storage, prioritizing the highest-value and hardest-to-replace items.
  • Raise machinery that can't be relocated onto platforms or sturdy industrial shelving.
  • Back up critical data and documents to a secure, off-site or cloud location.
  • Add waterproof enclosures to protect equipment that must stay in place.

 

Install Flood Barriers and Drainage Defenses

 

Keeping water out of the building is the heart of flood protection, and there's no single product that does it all. Most facilities layer several barrier types based on their building, budget, and risk. The table below compares the most common options.

 

Barrier Type Best For Strengths Considerations
Sandbags Low-cost emergency first line Inexpensive, widely available Labor-intensive, single-use, water can seep through
Sandless / Gel sandbags Rapid deployment, easier storage Lightweight until activated, compact to store Single-use, limited height per bag
Water-filled barriers Perimeters, driveways, entrances Reusable, fast to deploy, low labor Can be punctured; less effective on sloped or muddy ground
Flood panels, gates & doors Doors, windows, garages, loading docks Strong seal at specific openings Higher cost; may need pre-installed mounting hardware
Containment berms Encircling equipment; flood and spill control Reusable; contain water and spills Require open setback space
Drain covers & backflow preventers Floor drains and sewer lines Stop water backing up through drains Address one entry path; use as part of a layered defense

 

Pair these with good drainage practices. Keep gutters, storm drains, and floor drains clear so water has a path away from the building and install backflow preventers so sewers can't allow water back inside. Sump pumps at the lowest points of the building provide active removal of water that does get in, and a battery backup keeps them running if the power fails.

 

Secure Hazardous Materials

 

Floodwater that reaches chemicals, fuels, or other hazardous materials can spread contamination across your facility and into the environment, turning a flood into a far more serious and costly safety and environmental incident. The danger isn't only contamination, as some materials are water-reactive. Substances such as certain alkali metals react violently on contact with water, releasing heat and flammable or toxic gases and creating fire and explosion hazards.

 

Before a flood, move hazardous materials to higher ground where possible, ensure containers are sealed and stored on secondary containment, and keep spill response supplies accessible. Containment berms and spill kits do double duty here, helping to block incoming floodwater and contain any chemicals that escape, keeping them from mixing with the water and spreading contamination.

 

Protect Utilities and Power

 

Utility systems are among the most expensive things to repair after a flood. Where feasible, elevate or floodproof electrical panels, HVAC equipment, and mechanical systems, and protect electrical components with waterproof enclosures. Install check valves where utility and sewer lines enter the building. A check valve is a one-way valve that lets water and sewage drain out while preventing it from backing up into the building when municipal systems are overwhelmed. Also plan for backup power and lighting, such as generators and battery-powered lighting, so critical functions and safety equipment can keep running.

 

Build an Evacuation and Communications Plan

 

Build an Evacuation and Communications Plan

 

A flood safety plan protects the one thing that matters most: your people. A strong plan assigns clear roles and authority, defines evacuation routes and assembly points, and spells out shutdown procedures for equipment and utilities. It should also establish how you'll communicate and maintain current contact lists for personnel, suppliers, and emergency services. Train your team on the plan and run through it before flood season, not during a warning.

 

During a Flood: Acting Safely

 

When a flood is imminent or underway, the priority shifts from prevention to safety. Monitor official sources such NOAA Weather Radio, local emergency management, and FEMA, and act on warnings without delay. Execute your shutdown procedures for equipment and utilities, deploy any remaining barriers if it's safe to do so, and evacuate according to your plan when directed.

 

Above all, keep people away from floodwater. Never let employees drive or walk through flooded areas; even shallow moving water is dangerous, and floodwater can hide debris, downed power lines, and contamination. Account for everyone at your assembly point, and don't return to the building until authorities give the all-clear.

 

After a Flood: Recovery and Cleanup

 

How quickly and safely you recover has a direct effect on total cost and downtime. Work through recovery methodically.

 

Enter Only When It's Safe

 

Wait for an official all-clear before re-entering and treat the building as hazardous until you've confirmed otherwise. Water and electricity are a deadly combination; don't enter areas where water has reached outlets or the electrical panel, and never remove an electrical panel cover unless you're a licensed electrician. Assume floodwater is contaminated with sewage, chemicals, or debris, and wear appropriate PPE, including rubber boots, gloves, and respiratory protection, before going in.

 

Remove Standing Water

 

Once the building is safe to enter, remove standing water as quickly as possible. Submersible, utility, and trash pumps handle large volumes and deeper water, while wet/dry vacuums tackle what's left and squeegees push the rest toward drains or sump pits. Trash pumps are especially useful for flood cleanup because they're built to move debris-laden water (mud, leaves, twigs, and small solids) that would clog an ordinary pump. Make sure interior and exterior drains are clear of debris, so water has a clear path out.

 

Dry Out the Facility

 

Drying is a race against mold, which can begin to grow within 24 to 48 hours. As soon as standing water is gone, drop the humidity fast. Run dehumidifiers on their highest settings and position air movers or high-velocity fans to push air across wet floors and walls. Open doors and windows to ventilate when outdoor conditions allow. Remove and dispose of water-damaged porous materials like wet carpeting, drywall, insulation, and baseboards, since these trap moisture and create an ideal environment for mold to grow, even after surfaces appear dry.

 

Document everything with photos and a written inventory for your insurance claim before you discard anything. Where possible, record model and serial numbers as well, since these help with verification and ensure accurate replacement.

 

Inspect for Structural and Electrical Damage

 

Before fully reoccupying, look for warning signs of damage like foundation cracks, bulging or leaning walls, sagging materials, and other signs of structural compromise, along with any evidence of ruptured gas or electrical lines. A visual walk-through can catch obvious problems, but it is not a substitute for a professional inspection. Flooding can cause hidden damage to a building's structure, electrical system, plumbing, gas lines, and HVAC equipment that only qualified experts can properly assess.

 

Before restoring power or resuming operations, have licensed professionals inspect and clear the affected systems: a structural engineer for the building itself, a licensed electrician for the electrical system, and qualified technicians for plumbing, gas, and HVAC. Never turn the power back on until a professional has confirmed it is safe to do so, because energizing a flood-damaged electrical system can cause fire, electrocution, or further damage.

 

For guidance on what to look for and the hazards involved, Global Industrial's Knowledge Center article Flood Damage: Checking the Foundations is worth reviewing, but it is a supplement to professional inspection, not a replacement for it.

 

Prevent Mold and Secondary Damage

 

Even after the visible water is gone, hidden moisture behind walls and under floors can fuel mold and decay for weeks. Keep dehumidifiers and air movers running until materials are fully dry, verify dryness with moisture meters rather than by appearance, clean and disinfect surfaces that contacted floodwater. Staying ahead of moisture is what prevents a one-time flood from becoming a long-term mold and structural problem.

 

Equipment Checklist for Flood Preparedness and Recovery

 

Each phase of flood management depends on having the right equipment on hand before you need it. Use this as a planning checklist.

 

Stage Task Equipment
Before Block and divert water Sandbags, water-filled barriers, flood panels, containment berms
Before Prevent drain and sewer backup Drain covers, backflow preventers, sump pumps with battery backup
Before Protect assets and utilities Industrial shelving to elevate, waterproof enclosures, secondary containment
During Stay informed and protected Weather radio, backup power and lighting, PPE
After Remove water Submersible, utility, and trash pumps; wet/dry vacuums; squeegees
After Dry the facility Dehumidifiers, air movers, fans
After Work safely PPE (boots, gloves, respirators), moisture meters

 

Building Long-Term Flood Resilience

 

Flooding may not be fully preventable, but its impact is largely controllable. Facilities that assess their risk, invest in layered protection, secure their people and hazardous materials, and equip themselves for fast recovery consistently come through flood events with less damage, lower recovery and repair costs, and shorter downtime than those that improvise.

 

Global Industrial is a comprehensive resource for both sides of that equation: preparedness and recovery. From spill containment berms, sandbags, and spill control supplies for keeping water and contaminants out, to pumps, sump pumps, dehumidifiers, wet/dry vacuums, air movers, and PPE for cleanup, equipping your facility from a single source makes it far easier to build a plan you can actually execute when it counts.

 

The best time to prepare for a flood is long before one is in the forecast. Put the plan and the equipment in place now, and you protect your people, your property, and your operations for whatever the weather brings.

 

Frequently Asked Questions

 

How can a business prepare for a flood?

 

Effective flood preparedness starts with assessing your flood risk, then elevating and protecting equipment, inventory, and records; installing flood barriers and drainage defenses; securing hazardous materials and utilities; and building an evacuation and communications plan. Having the right equipment on hand before a flood and training your team on the plan makes the difference between an orderly response and a scramble.

 

What are the best flood barriers for commercial buildings?

 

There's no single best barrier; most facilities layer several. Sandbags and sandless gel bags are inexpensive first lines of defense; water-filled barriers offer reusable perimeter protection; and flood panels, gates, and doors seal specific openings like entrances and loading docks. Containment berms protect equipment and contain both water and spills, while drain covers and backflow preventers stop water from backing up through drains. The right mix depends on your building, budget, and risk level.

 

What equipment is needed to remove flood water?

 

Removing flood water typically calls for submersible, utility, or trash pumps for larger volumes and deeper water, wet/dry vacuums for what remains, and squeegees to direct water toward drains or sump pits. After the water is gone, dehumidifiers and air movers are essential for drying the space and preventing mold. Crews should wear PPE throughout, since floodwater is often contaminated.

 

What should be in a flood safety plan?

 

A flood safety plan should assign clear roles and authority. It should also define evacuation routes, assembly points, and detail shutdown procedures for equipment and utilities. It should also establish communication protocols for how alerts reach employees and where they get updates. Make sure to maintain current contact lists for staff, suppliers, and emergency services. Train your team on the plan and practice it before flood season.

 

Is it safe to enter a building right after a flood?

 

Not until it's been cleared. Wait for an official all-clear, and stay out of areas where water has reached electrical outlets or panels because of electrocution risk. Treat floodwater as contaminated, wear protective gear, and watch for structural damage, broken gas lines, and downed or exposed power and utility wires. Leave panel covers and serious structural or electrical inspection to licensed professionals.

 

Does commercial property insurance cover flood damage?

 

Often it does not. Standard commercial property policies typically exclude flood damage, which is usually covered through separate flood insurance such as the National Flood Insurance Program. Because such coverage commonly carries a waiting period of around 30 days before it takes effect, it's worth reviewing your coverage well ahead of flood season rather than when a storm is approaching.

 

The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial be liable for any loss or damage caused by your reliance on this article.