Fan Dolly for Pedestal Fans - fits 1-1/2" to 2-1/4" dia. columns and 28" and smaller bases

Rollover image to zoom in

Click image to enlarge

See all 2 items in product family

Fan Dolly for Pedestal Fans - fits 1-1/2" to 2-1/4" dia. columns and 28" and smaller bases

Item #: WB245658

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Qty Price
1-5 $29.95 ea.
6+ $24.95 ea.
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
FAN DOLLY FOR PEDESTAL FANS
Converts pedestal fans into mobile floor fans for easy portability from site to site. Dolly is made of 1“ x 2“ x 18 gauge tubular steel legs on 16“ centers. Two 6“ x 1-1/2“ non-marring rubber wheels with bolt-on plastic hub allow easy mobility when pedestal fan is tilted. Fan dolly includes post collar and bracket to easily fit onto 1-1/2“ to 2-1/4“ dia. pedestal columns with 28“ diameter or smaller base. Hardware included.

Product Specifications

    • BRANDGlobal Industrial™
    • ASSEMBLYUnassembled
    • DEPTH INCHES16
    • MANUFACTURER'S PART NUMBER245658
    • COLOR FINISHBlack
    • CONSTRUCTIONSteel
    • FAN TYPEIndustrial
    • DESCRIPTION6" x 1-1/2" Non-Marring Rubber Wheel Plastic Hub
    • MODEL245658
Have A Question About This Product?
1 Question | 1 | Answer

Avg. Customer Rating: (47 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating
Sort by: 
1 2 ...

47 Results

receiving mgr.

Your review: it seems to be holding up well

Pros: it helps moving the fan from 1 area to another

Cons: none

Is this review helpful?

Fan Dolly

Your review: It is great!!!

Pros: It does the heavy work for you... great item.

Is this review helpful?

Pedestal fans

Your review: great fans definitely moves a lot of air with the wheel attachment it is easy to maneuver around

Pros: with the desperate wheel attachment they are easy to move

Cons: I wish it had a spot to roll the cord up on

Is this review helpful?

Main. Mgr.

Your review: Works great easy to move fan around.

Is this review helpful?

Nice add-on

Your review: The dolly was easy to attach and works perfectly.

Pros: Easy to attach, Universal

Cons: None

Is this review helpful?

Great addition to a fan

Your review: These are fairly well built my only recommendation would be to have a better wheel one with a bearing

Is this review helpful?

Great idea !

Your review: Easy moving shop fans around with this dolly attachment. No longer a two man job.

Pros: Easy to install and easy to move fans around.

Cons: None for me.

Is this review helpful?

Great addition

Your review: Sturdy well built unit that makes moving around my cumbersome 30" pedistal fan a snap. Highly reccomended if you have the need to frequently move your fans fro location to location.

Pros: Well built unit-great fit.

Cons: A little pricey, but worth it.

Is this review helpful?

A needed accessory for the fan

Your review: Easy assembly, functional, meets its objective

Pros: Allows moving the fan with ease

Cons: none

Is this review helpful?

awesome!

Your review: loved the wheels 4 our fan; in fact, our church's fan....got a pair also. much easier to move! THANKS!!!

Pros: :0)

Cons: none!

Is this review helpful?

Buy These

Your review: If you bought or are going to buy one of their pedestal fans, these things are great! And they're pretty inexpensive too.

Is this review helpful?

The photo doesn't do it justice

Your review: This 'fan dolly' is more 'hefty' than what it appears in the photo. Its built extremely well and is a must if you plan on moving the pedestal fan around.

Pros: Very will built

Cons: None

Is this review helpful?

Just Right!

Your review: Bought it to go on my pedestal fan ... now I can move the fan anywhere I want easily.

Is this review helpful?

Fan dolly

Your review: Works as expected.

Pros: Appears to be sturdy and well built

Cons: Hex head bolts make it more difficult to assemble.

Is this review helpful?

Received As Described And On Schedule

Your review: I am very impressed with the order and delivery.The item arrived better than described, more robust than described. I am very pleased.

Pros: Great customer service phone operators, great service throughout.

Cons: Absolutely none.

Is this review helpful?

Seems like a necessary add-on

Your review: I would attach 'highly recommended' to the dolly whenever anyone orders the pedestal fan as there's no easy way to move the fan without it. Works great!

Pros: Easy to attach. Works as designed.

Cons: None.

Is this review helpful?

Fan Dolly for Pedestal Fans

Your review: Very sturdy construction. I was surprised at the mounting, which places the dolly frame parallel and 7" above the fan base, with the wheels 5" above the base. This requires the fan to be tilted 60°-80° before the wheels carry the weight ofthe fan. The dolly works, but is truly useful only when the fan must be moved a considerable distance.

Pros: Adequate for moving the fan more than a foot or two.

Cons: Usefulness is only realized on moves of several feet. For short moves, it's better to skid or roll the fan base to the new position. The dolly serves no purpose for moves of only a foot or two.

Is this review helpful?

Fan Dolly

Your review: Great Product. Easy to install.

Pros: All good.

Cons: None

Is this review helpful?

Best To Buy This, Too!

Your review: This simple dolly attachment makes moving my pedestal fan much easier than otherwise. The fans are sturdy and heavy and their large supportive base makes tipping the fan difficult and sliding it along whatever surface will not be fun or free from causing abrasions. The instructions are the 'visual' kind and it is important to note that a polymer flange is included in the package that is not needed if the pole on your unit is the thicker kind. I failed to initially notice the either/or instruction just above the two pictures showing alternative products. The dolly does secure firmly to the pedestal when the clamp parts are well-tightened and the fan then becomes mobile! The metal frame is strong and doesn't flex under load. The wheels are not 'over-engineered' but they work smoothly. The axle screws/bolts are heavy-duty enough to support the load of the fan during occasional changes in location.

Pros: Adds important functionality to a pedestal fan. Well-built for its intended use. Assembles easily using basic tools (adjustable wrench, screw driver set.)

Cons: None have cropped up yet.

Is this review helpful?

FAN STAND

Your review: GREAT PRICE FAST DELIVERY

Is this review helpful?

Fan Dolly

Your review: A must have for the tall pedestal fans

Pros: Real easy to move big fan.

Cons: none

Is this review helpful?

Fan Dolly

Your review: Love it...heavy fan much more portable.

Pros: strong construction

Cons: instructions a bit sketchy.

Is this review helpful?

Fan dolly

Your review: This dolly is well made, and assembly is fast. A big help when moving a pedestal fan around on smooth, as well as moderately rough, but firm surfaces.

Pros: Value priced. Easy assembly. Quality materials.

Cons: None.

Is this review helpful?

Fan Dolly

Your review: Easy to install work well for easy movement of fan.

Pros: Easy install, works as stated.

Cons: None

Is this review helpful?

Sort by: 
1 2 ...

47 Results

There are 47 questions and 1 answers for this product.

Sort by: 
1 2 ...  

47 Results

WHAT IS THE LARGEST DIAMETER FAN AND LARGEST HP THAT BE USED WITH THIS STAN BEFORE IT WILL TRUN OVER? THAT IS RUNNING ON HIGH SPEED.

Question Asked By: JOE , METTER, GA , July 20, 2017

+ View 1 Answer

Answer This Question

Sort by: 
1 2 ...  

47 Results