Blue LED Forklift Pedestrian Safety Warning Spotlight

Rollover image to zoom in

Click image to enlarge

See all 6 items in product family

Blue LED Forklift Pedestrian Safety Warning Spotlight

Item #: WB988717

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $74.95 Save up to 48%
Promotion Price: $ 39.00

with FREE shipping today! (within the contiguous US)

Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
BEST VALUE BLUE LED FORKLIFT PEDESTRIAN SAFETY WARNING SPOTLIGHT

Promote Worker & Pedestrian Safety!

When the LED Safety Warning Spotlight assembly is mounted to a forklift or other moving vehicle, it projects bright blue spot beam pattern on the floor surface. Since multiple lights can be mounted onto a single fork lift truck, the warning light spots can be seen behind or in front of the forklift. The bright light spot on the floor is clearly visible to pedestrians, machines and vehicles in the area, regardless of the ambient noise, alerting them to the nearby presence of the forklift. Traditional audio back up alarms can blend into ambient noise in the building and pedestrians can become immune to the audio warning.

Twin 5 watt solid-state, shock-resistant, Cree LED (Light Emitting Diode) lights yielding 600 lumens are enclosed in an IP68 rated housing with a UV-resistant PMMA polycarbonate lens. The LED forklift safety light uses the vehicle electrical power to operate and can be installed on the front and/or rear of any forklift, sweeper, AGV or industrial vehicle (configured for 10 Volt to 80 Volt DC input range, with reverse voltage protection). The 50,000 hour service life LED's are mounted in a rugged die-cast aluminum housing for long life. Working environment temperature is -31 to 185° F. Universal stainless steel swivel mounting bracket allows for easy installation. 1 Year Limited Warranty.

Note: Configured for 10 to 48 Volt DC input:
0.550 amps @ 12V DC
0.280 amps @ 24V DC
0.180 amps @ 36V DC
0.140 amps @ 48V DC

Documents

Documents are in PDF format

Product Specifications

    • LENGTH INCHES6-1/2
    • WIDTH INCHES4
    • HEIGHT INCHES4-3/4
    • COLOR FINISHBlack
    • # LED's2
    • APPROVAL/REGULATIONSIP68
    • ASSEMBLYAssembled
    • BRANDGlobal Industrial™
    • CONSTRUCTIONDie-Cast Aluminum Housing, PMMA Lens
    • LIMITED WARRANTY1 Year
    • LUMENS600
    • MANUFACTURERS PART NUMBER988717
    • MOUNTING TYPEUniversal
    • POSITION ON FORKLIFTFront and/or Rear
    • SPOT OR LIGHT BEAM COLORBlue
    • TYPELED Forklift Safety Warning Spolight
    • VOLTAGE10 - 48
    • WEIGHT LBS1.8
    • WORKING TEMPERATURE-31 to 185° F
Have A Question About This Product?
3 Question | 3 | Answer

Avg. Customer Rating: (35 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

A great safety tool!

Good value. Great price (our service company would have charged a lot more to provide one). Easy installation, great operation.

See more favorable reviews

The most critical review

  • Customer Rating
Sort by: 
1 2 ...

35 Results

A great safety tool!

Your review: This is an easy to install item that enhances your warehouse safety immensely. The projected blue light is an attention getter, especially when people become "ear blind" to the reverse alarm beeping. Ours are aimed 10' behind the forklift, and all the warehouse staff has commented on how useful it is.

Pros: Good value. Great price (our service company would have charged a lot more to provide one). Easy installation, great operation.

Cons: Can't think of any.

Is this review helpful?

Very good unit for a fair price

Your review: Very good unit for a fair price

Pros: Easy to install

Is this review helpful?

Great for Safety

Your review: Great for safety and great price.

Is this review helpful?

Warning lights

Your review: Really like the projection these lights. Have them installed on front and rear of vehicle.

Pros: Advanced warning of approaching traffic.

Is this review helpful?

Blue LED Forklift warning light

Your review: Works great.

Pros: Potential injury avoidance/ life saver.

Cons: Need to install 2 per fift.

Is this review helpful?

Maintenance Planner/Scheduler

Your review: Bright Blue light

Is this review helpful?

Purchasing Specialist

Your review: Customer Service is always a pleasure to work with.

Is this review helpful?

Maintenance Manager

Your review: Just what we needed

Pros: Makes individuals aware of forklift

Cons: NONE

Is this review helpful?

Excellent Lights

Your review: We installed these and have had excellent results!

Pros: The light is very , very bright. It captures pedestrian's attention ASAP! I t reflects off of our plastic wrapped finish goods in the warehouse so you always know where your drivers are.

Cons: None

Is this review helpful?

PURCHASING MANAGER

Your review: THIS WAS PURCHASE AS A SAFETY ITEM TO BE MOUNTED ON OUR LIFT TRUCKS. THEY'RE VERY BRIGHT AND APPEARS TO BE SERVING IT'S PURPOSE.

Pros: ANY TIME YOU CAN KEEP ANYONE FROM GETTING HIT BY A FORK LIFT, THAT'S DEFINITELY WHAT YOU WANT.

Cons: NONE TO THANK OF.

Is this review helpful?

Blue LED Pedestrian Safety Warning Lights

Your review: We purchased these for front/rear visibility in a Warehouse that has many blind corners.

Pros: The blue light draws attention ASAP! It reflects off of all of our plastic wrapped pallets allowing us to know where our lifts are at all times!

Cons: None, if you don't have them then you are shorting yourself and your Company on it's safety program!!

Is this review helpful?

Safety light

Your review: We have been using these lights for years and show up great on the warehouse floor.

Pros: Bright, easy to install and long lasting

Cons: The price has gone up a few times. It needs a clamp attachment because you can't drill into overhead protection.

Is this review helpful?

safety lights

Your review: Purchased these safety lights for use in an industrial business on forklifts. They are an excellent choice- high visibility and an excellent price in comparison to other similar warning lights.

Pros: price and durability

Cons: none that I am aware of as of yet

Is this review helpful?

Safety Blue

Your review: We have made several safety improvements over the years that employees see as another barrier to their job. However, this improvement has had the reverse effect. Employees comment on how much safety they feel with the blue lights on the forklifts. If the forklift operator does not sound their horn, they still no that they are present due to the blue light.

Is this review helpful?

Work Exactly How They Should

Your review: Like I said, these lights work exactly how they should on our forklifts. The blue light shines bright on the floor in both incandescent and LED overhead lighting. They are especially helpful in our plant because we have electric forklifts, and they are hard to hear coming with the surrounding factory noise.

Is this review helpful?

Blue LED Forklift Pedestrian Safety Warning Spotli

Your review: bright and clear, rugged, easy to install. will repurchase as needed

Cons: none

Is this review helpful?

Fork Lift Blue Safety Light

Your review: I had these blue lights intalled on our fork lifts and I am very happy with them. I feel as though the folks are more aware of the vehicle traffic in the warehouse now as they are noticing the blue lights on the floor as they move around.

Pros: High visibility, increased safety and awareness

Cons: Sometimes the light moves from it's position and you have to readjust.

Is this review helpful?

Good item

Your review: Very bright, focused beam, durable case

Is this review helpful?

Safety LED Lights

Your review: A must have in the warehouse. Great addition to any lift to promote the maximum safety.

Is this review helpful?

BLUE PEDESTRIAN SAFETY LIGHT

Your review: This warning light works very well. It shines on the floor ahead of or behind the lift. When a pedestrian sees this light on the floor it make them stop and see where the light is coming from. #RP1988717 is not the brightest of this type of light that is sold. It is plenty sufficient though. An excellent value.

Pros: Excellent pedestrian safety. Bright enough. Everything needed to mount the light is included. Excellent value.

Cons: Not the brightest available.

Is this review helpful?

Pedestrian Safety Light

Your review: Very good light to try to warn pedestrians of a forklift coming. Shines bright blue oval on floors. This model is not the brightest out there but it is plenty bright to do the job.

Pros: Long lasting. Bright enough. Easy to install. Uses little power to run.

Cons: No cons to be aware of.

Is this review helpful?

Purchasing Agent

Your review: We tested this product on one of our fork trucks and the very first day it saved ME! An electric fork truck that is very quiet,I did not hear or see but, that bright blue beam was 15' ahead of it around a blind corner! I almost stepped in front of the truck. We have installed forward AND rear facing light systems to maximize the safety benefit on our 8 fork and roll clamp trucks at our commercial printing plant. So far we have been very pleased with them. It is a great safety feature for the price!

Pros: adjustable distance and very bright!

Cons: Can't think of anything. We received soon after ordering them and our maintenance crew installed by the next day or two.

Is this review helpful?

Pedestrian warning

Your review: Alerts pedestrian about approaching forklift in a loud area.

Pros: Blue lights excellent

Cons: Need another light color for forward motion

Is this review helpful?

The Blue Light

Your review: These are a great safety item for your forklift. If you have deep aisles that you have to back out of or even backing away from a truck after loading a pallet this blue light is a great visual warning that the forklift is in reverse gear either moving or about to move. So many times you can hear the lift but not sure where it is coming from or there is multiple lifts in the area, this will allow you to pin point which lift is backing up.

Pros: Places a warning light on the ground behind the lift when in reverse. Can be adjusted to the distance you want to give warning to people or other lifts that a forklift is coming toward you in backward motion.

Cons: Wire connections should be round tube shape instead of flat spade connectors. This would make it a plug and play for the forklifts that Toyota makes.

Is this review helpful?

Sort by: 
1 2 ...

35 Results

There are 35 questions and 3 answers for this product.

Sort by: 
1 2 ...  

35 Results

How easy is it to install?

Question Asked By: Alex , July 11, 2019

+ View 1 Answer

Answer This Question

Can you provide a better price if purchasing 75+ blue lights? Also please provide warranty details for this product.

Question Asked By: Daniel Craven , Albany, Ga , September 04, 2015

+ View 1 Answer

Answer This Question

Can you provide a IP-68 certification for the forklift spotter light ?

Question Asked By: anonymous

+ View 1 Answer

Answer This Question

Sort by: 
1 2 ...  

35 Results

Customers Who Viewed This Also Viewed