It’s hard to keep your cool when dealing with the cleaning and maintenance of Packaged Terminal Air Conditioners. PTACs are notoriously hard to maintain. These commercial-grade units - typically installed directly through a wall - require annual attention to uphold indoor air quality (IAQ), reduce energy consumption, and prolong lifespan. When you have multiple units to clean, the task can be overwhelming.
Let’s face it - PTAC maintenance is cumbersome. It is a time-consuming process requiring multiple people. Regular cleaning - particularly in a hospitality environment - can take staff away from other pressing tasks. It is natural that this would lead to deferred maintenance. Unfortunately, neglecting PTAC maintenance can lead to multiple issues. A dirty PTAC strains to circulate air efficiently. The increase in airborne pollutants creates a potential health hazard. Plus, a dirty PTAC uses more energy and diminishes the unit’s longevity. The longer you defer hospitality maintenance, the less efficient the PTAC unit, leading to a shorter lifespan. In short, it is not the smartest place to cut corners.
Conversely, routine maintenance not only enhances air quality but also extends the lifespan of the unit, safeguarding your investment in the long run. But how can you balance the long term maintenance with the short-term personnel challenges? Enter the innovative solution: the EDIC PTAC Cleaning Cradle™. It’s a game changer.
One-Person Job: Saves Time and Money
In the past, cleaning PTAC units has been a labor-intensive task. Multiple personnel over many hours toil away on every nook and cranny. With the introduction of the PTAC Cleaning Cradle™, this process becomes a one-person job, saving both time and money. By minimizing the onsite workforce needed, property owners and cleaning contractors can enhance efficiency and realize significant cost savings. This efficiency translates to a quick return on investment, making the PTAC Cleaning Cradle™ an indispensable asset in any maintenance arsenal.
Unlike traditional cleaning processes, the PTAC Cleaning Cradle™ is a self-contained solution designed for a single operator to perform a deep cleaning right in the room. Here’s how it works: the patented design allows for the user to employ the adjustable jacks to quickly remove the unit from its wall sleeve. No more heavy lifting from multiple staff members. A formerly arduous task only takes minutes!
Why the EDIC PTAC Cleaning Cradle™ is a Game Changer

The EDIC PTAC Cleaning Cradle™ revolutionizes PTAC maintenance with its innovative design and unparalleled functionality. Engineered for ease of use by a single operator, this self-contained solution simplifies the deep clean process right in the room. Here are some key features that set it apart:
- Built-In Jacks: Dual jacks allow for easy adjustment - up and down, left and right. Vertical adjustments from 2.5” to 16” means no more heavy lifting! It’s a one-person operation!
- Tilt Functionality: A quick pin release enables effortless tilting of the cradle forward or backward, ensuring safety and convenience during cleaning.
- Integrated Casters: With casters on both jacks, transportation between locations becomes effortless, enhancing mobility and versatility.
- Vacuum Connect: The built-in vacuum hose clamp facilitates seamless connection to any portable extractor machine with a wet and dry vacuum system, streamlining the cleaning process.
- Durable Construction: Crafted from high-quality stainless steel, the PTAC Cleaning Cradle™ boasts durability and longevity, minimizing wear on parts and ensuring reliable performance.
- Eco-Friendly: As a "Green product," it aids in reducing electricity consumption, mitigating mold spores and fungus, and enhancing overall PTAC efficiency, promoting environmental sustainability.
Flexible for Your Needs
Cleaning PTAC units is not just a hospitality industry issue. In addition to hotels and motels, condominiums, nursing homes, apartments, hospitals, classrooms, and many more often have difficult, time consuming PTAC units to manage. The versatility of the PTAC Cleaning Cradle™ extends across just about any setting. Regardless of the PTAC's age or placement within the room, this design ensures thorough cleaning and optimal performance, enhancing customer satisfaction and peace of mind.
The EDIC PTAC Cleaning Cradle™is ONLY available through Global Industrial. This cutting-edge product exemplifies excellence in design, functionality, and performance. Whether you're a property owner, cleaning contractor, or maintenance professional, investing in this innovative solution promises to optimize efficiency, reduce costs, and enhance overall satisfaction. To learn more, talk to our Global Industrial team.
The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.