Key Takeaways
- Water expands about 9% as it freezes, and that pressure is what cracks and bursts a pipe, so frozen pipe prevention is about keeping vulnerable lines above freezing.
- Insulation slows heat loss but does not add heat.
- High-risk lines need heat trace cable to warm the pipe, sealed air gaps to keep cold drafts off it, and either a steady trickle of water or complete draining.
- Ice damsform when heat escaping into the roof melts snow that refreezes at the cold eaves. They can be prevented with attic insulation, ventilation, gutter clearing, and snow management.
A burst pipe or an ice dam can shut a facility down as fast as any storm. Unlike flooding, though, this damage comes from inside the building when temperatures drop, which is exactly why it catches so many facilities off guard.
According to the Insurance Institute for Business and Home Safety, burst pipes are one of the most common causes of property damage during freezing weather, and a single failure can release water into offices, warehouses, production areas, and electrical rooms for hours before anyone notices. This guide focuses on the two highest-stakes cold-weather failures, frozen pipes and ice dams, and the commercial freeze protection steps that prevent them.
Why Freezing Damages a Facility From the Inside
When water in a pipe freezes, it expands by about 9 percent. A pipe rarely bursts where the ice forms, however. The ice acts as a plug, and as freezing continues, it pressurizes the water trapped between the plug and a closed faucet or valve. The pipe then fails at its weakest point, which may be well away from the ice and out of sight. The rupture may not show until the ice thaws, when water flows out from inside a wall, ceiling, or mechanical room.
Temperature is the trigger. Water begins to freeze at 32 degrees Fahrenheit, but the burst risk climbs sharply once exposed pipes see sustained temperatures below about 20°F for several hours, especially when wind or drafts are present. Poor insulation accelerates the process further.
There is a budget and compliance angle worth knowing, too. Insurance coverage for frozen-pipe damage generally depends on the building having been kept heated and on reasonable care being taken to prevent freezing, so a claim can be denied when heat was intentionally left off or a vacant zone was neither heated nor drained. Prevention is not only cheaper than repair; it is often what keeps a loss covered at all.
How to Prevent Frozen Pipes
Knowing how to prevent frozen pipes starts with identifying which ones will freeze first, then applying the right protection to each.
- Identify the lines most at risk. Freezing targets pipes that run through unheated or poorly heated spaces, such as attics, crawl spaces, basements, mechanical rooms, and remote or rarely used areas, along with any line in an exterior wall. Dead legs and unused lines with no water movement are especially vulnerable, and smaller-bore pipes freeze faster than large ones because they hold less water. Walk the building and map these before the first hard freeze.
- Choose between insulation and heat tracing. This is the decision that matters most, and the key fact is that insulation slows heat loss but adds no heat of its own. An insulated pipe will still freeze given enough sustained cold, so insulation alone suits lines that stay reasonably warm and only need their heat retained. For high-risk lines, exposed piping, unheated spaces, dead legs, and anything facing deep sustained cold, heat trace cable is the answer. Heat trace, also called heat tape, runs along the pipe and adds heat directly, held at a setpoint by a thermostat so it energizes only when needed. Best practice pairs the two, running heat trace cable under insulation so the insulation retains the cable's heat and cuts its energy use.
- Keep water moving or drain unused lines. Moving water is far harder to freeze than still water, so letting vulnerable fixtures run a small trickle during extreme cold is a proven stopgap. For lines that will not be used through the winter, or for zones being shut down, the better answer is to drain them completely so there is no water left to freeze.
- Seal cold-air gaps near piping. A pipe in a heated space can still freeze if cold outside air is leaking directly onto it. Seal cracks and penetrations in walls, at sill plates, and around windows and doors near vulnerable piping. Close off drafts into cabinets and chases where supply lines run.
- Maintain heat everywhere, including unoccupied areas. Keep interior temperatures above about 55°F around the clock and resist deep overnight or weekend setbacks in spaces with plumbing. The areas most often skipped, such as remote wings and unoccupied zones, are the ones that fail.
- Know how to safely thaw a pipe that has frozen. If a fixture produces only a trickle, a pipe is likely frozen. If you suspect it has already burst, shut off the main water supply first. Open the affected faucet to relieve pressure and to confirm melting as flow returns, then apply gentle heat, starting at the faucet side and working toward the blockage. A portable space heater, a heat gun or hair dryer on low, a heating pad, or warm towels all work, as does dedicated heat trace cable. Never use an open flame or torch, which can damage the pipe and start a fire. If the pipe is inaccessible or has burst, call a licensed plumber. Acting quickly matters, since fast response can cut total water damage considerably.
Global Industrial carries pipe and plumbing insulation, heat trace and pipe heating cable, and portable heaters for warming enclosed spaces during a thaw, along with blanket and band heaters for protecting tanks, drums, and totes.
How to Prevent Ice Dams
An ice dam is a ridge of ice that forms at the edge of a roof and stops melting snow from draining, and understanding how to prevent ice dams starts with why they form. Heat escaping from the building into the roof or attic warms the upper roof surface and melts the snow sitting on it. That meltwater runs down toward the eaves and overhangs, which stay cold because no heated space sits beneath them, and there it refreezes into a growing dam. Water then pools behind the dam and backs up under the shingles, where it works its way into the building. The fix is to keep the roof surface uniformly cold and to give meltwater a clear path off the roof.
- Air-seal and insulate the attic or roof assembly. Seal gaps around hatches, ducts, light fixtures, and other penetrations using materials appropriate for each location. Then evaluate insulation to reduce heat transfer to the roof deck. Maintain ventilation suited to the roof design as a supporting measure. Assess attic piping separately, since these improvements do not automatically protect pipes outside the heated building envelope.
- Clear gutters and drainage. Clogged gutters and downspouts give ice a place to build, so clearing them before winter keeps meltwater moving. On low-slope commercial roofs, keep roof drains and scuppers clear for the same reason.
- Manage snow load. Removing snow from the roof edge with a roof rake after heavy storms takes away the material that feeds a dam, and it also addresses the separate risk of excess snow load on the structure.
- Add heat cable where needed. Self-regulating roof and gutter de-icing cable at the eaves, valleys, and downspouts maintains a melt path through the dam-prone zone. It is the same heat trace and roof and gutter cable family used for pipe freeze protection.
Freeze Detection: Catching a Failure Before It Floods
Prevention reduces the odds of a freeze, and detection limits the damage when one happens anyway. The failures that cost the most tend to strike where no one is looking, such as an unoccupied wing, a remote mechanical room, or the whole building over a weekend or during a holiday break.
Low-temperature alarms and remote temperature monitoring track those zones continuously and send an alert when a space drops below a set threshold. That gives staff time to restore heat or drain a line before a pipe freezes and bursts. Water-leak sensors complement temperature monitoring by detecting water on the floor near water heaters, supply lines, and other plumbing. Many can be connected to an existing intrusion or fire alarm panel, so a leak triggers the same alert and monitoring response as any other alarm. Automatic shut-off valves go a step further and close the water supply when a leak is detected, which limits damage even when no one is on site.
Building a Freeze-Protection Plan
Effective freeze protection is a seasonal routine, not an emergency response. Before winter, identify the vulnerable lines and zones in the facility. Insulate lines that only need to retain their heat, install heat trace cable on lines that need heat added, and seal the air gaps that let cold air reach them. Keep water moving in vulnerable lines that remain in use, and drain lines that will sit idle. Maintain heat in every space that contains plumbing, including unoccupied areas. On the roof, address insulation, ventilation, gutters, and snow removal. Finally, install monitoring in the zones staff cannot check in person.
Facilities that complete these steps before the first hard freeze are far less likely to experience a burst pipe or ice dam during the season.
Pre-Winter Freeze-Protection Checklist
Plumbing
- Walk the building and map every line in unheated spaces, exterior walls, and rarely used areas, including dead legs.
- Inspect pipe insulation, and repair or replace any that is damaged, wet, or missing.
- Install heat trace cable on high-risk lines, and test existing cable and thermostats.
- Drain and shut off lines that will not be used through the winter.
- Locate and label the main water shut-off valve, confirm it operates, and make sure staff know where it is.
Building envelope and heat
- Seal cracks and penetrations near vulnerable piping, including wall penetrations, sill plates, and the areas around windows and doors.
- Set thermostats to maintain at least 55°F in all spaces with plumbing, including unoccupied zones.
- Limit overnight and weekend temperature setbacks in those spaces.
Roof
- Inspect attic or roof-space insulation and ventilation.
- Seal air leaks around light fixtures, hatches, ducts, and other roof penetrations.
- Clear gutters, downspouts, roof drains, and scuppers.
- Test roof and gutter de-icing cable.
- Stage roof rakes and arrange snow removal for heavy storms.
Monitoring and response
- Install and test low-temperature alarms and remote temperature sensors in the coldest areas.
- Install and test water-leak sensors and automatic shut-off valves.
- Confirm who receives alerts and how they will respond after hours, on weekends, and over holidays.
- Document each completed step to support any future insurance claim.
Global Industrial supplies the equipment each step requires, from pipe insulation and heat trace cable to blanket heaters and ice removal essentials. Having that equipment in place before the first freeze reduces the risk of an unplanned shutdown.
Frequently Asked Questions
Is pipe insulation enough to prevent freezing on its own?
Not always, and this is the most common misunderstanding. Insulation slows the rate at which a pipe loses heat, but it adds no heat of its own, so an insulated pipe will still freeze if the cold lasts long enough. Insulation is the right protection for lines that stay reasonably warm and only need that warmth retained. For exposed pipes, unheated spaces, dead legs, or deep sustained cold, you need heat trace cable to actively add heat, ideally installed under insulation so the two work together.
Should I let faucets drip or drain the lines?
It depends on the line. For vulnerable but in-use fixtures during an extreme cold snap, letting a small trickle run keeps water moving and is much harder to freeze than still water. For lines that will sit unused through the winter, or in zones being shut down or left vacant, the better move is to drain them completely so there is nothing left to freeze. Dripping buys short-term protection; draining removes the risk entirely.
Does insurance cover frozen pipe damage?
In most cases yes, but with an important condition. Most policies treat a burst frozen pipe as a covered, sudden loss only if the building was being heated and reasonable care was taken to prevent freezing. Coverage can be denied when heat was intentionally shut off, or when a vacant zone was left neither heated nor drained. That makes documented freeze-protection steps, maintained heat, and monitoring a matter of protecting the claim as well as the property. Review those requirements with your insurer or broker before winter.
What should I do first if a pipe has already burst?
Shut off the main water supply immediately to stop the flow, then cut power to any affected area where water is near electrical equipment, since water and electricity together are a shock and fire hazard. Move records, servers, and equipment out of the water, begin removing standing water, and document everything for the insurance claim. Arrange prompt professional water removal and drying. EPA recommends drying water-damaged areas and materials within 24–48 hours to help prevent mold growth [1].
Can the same heat cable protect both pipes and gutters?
Some heating cables are approved for both pipe freeze protection and roof-and-gutter de-icing. Confirm that the specific model is approved for the intended application and follow its installation instructions.
References:
- U.S. Environmental Protection Agency. (n.d.). How do I get rid of mold? https://www.epa.gov/mold/how-do-i-get-rid-mold.
The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial be liable for any loss or damage caused by your reliance on this article.