JET® Blade Guide For Wilton And Jet Band Saws
Write a Review
Questions & Answers (0)
Blade guide for Wilton and JET band saws. Carbide. Keeps blade straight for cutting. See model diagram for installation.
Specifications
Product Details
| Manufacturers Part Number | JT9-5783391 |
| Type | Blade Guide |
| For Use With | Band Saws, Saws |
| Package Quantity | 1 |
| Description | Guide Block Carbide |
| Brand | JET |
Related Products
This is a genuine OEM replacement table Insert used on Jet band saws. Table Saw Inserts reduce splintering and chip-out on the cuts. It also prevents thin slices of wood from jamming in between the blade and the plate during a cut. If an insert is missing or damaged it needs to be replaced. This part is made out of metal and it is sold individually. For Use With: Jet JWBS-14DXPRO Delux Pro Band Saw JWBS-14DXPRO Delux Pro Band Saw JWBS-14CS (708115K) 14-inch Woodworking Band Saw JWBS-14CS (708115K) 14-inch Woodworking Band Saw JWBS-14OS (708113A) 14-inch Woodworking Band Saw JWBS-14OS ...
This is an original Jet-Wilton replacement part. The metal blade wheel is used in bandsaws to hold and turn the circular saw blade. You may want to replace both the front and rear blade wheels at the same time for even wear. If the blade wheels on your band saw have a tire, please be aware that the blade wheel does not come with the tire installed, so you may also want to purchase a new tire. You will need a hex or Allen wrench to replace this item. For Use With: Jet J-3410-2 (414455) 7x12 Cut-off Bandsaw J-3410-2 (414455) 7x12 Cut-off Bandsaw J-3410 (414454) 7x12 Cut-off Bandsaw J-3410 ...
It is a genuine item that is supplied by the original manufacturer for use with Jet and Wilton bandsaws. This is the special center shaft that helps to secure the blade. It provides an identical replacement for a damaged or a missing component that was installed on a new unit. Ensure the correct installation of the new part by referring to the owners manual and the appropriate diagrams of your specific model. Note, this high-quality shaft is made of durable metal and is sold individually. For Use With: Jet J-7020M (414474) 10"x16" Miter Cut-Off Bandsaw J-7020M (414474) 10"x16" Miter ...
This item is a genuine part that has been sourced from the original manufacturer to be used with verticle bandsaws from Wilton and Jet. The durable plastic insert fits into the cap in the table where the blade passes through the table. The insert is used to reduce the gap around the blade in order to better support the material as it is being cut. Inserts wear down from normal use, and will eventually need to be replaced to maintain clean accurate cuts. This part is priced as a single item, please note tools may not be necessary to install the insert. For Use With: Jet 8201 (9078171) ...
This is a genuine OEM supplied component which is specially made for use with Jet and Powermatic band saws. The tire is one of the most important parts of a bandsaw. Its purpose is to help track the blade on the wheel. Unfortunately, over time the material will wear out and it may begin to crack eventually requiring a replacement to ensure peak performance. Keep in mind this high-quality tire is made of durable rubber and is sold individually. Please make sure to refer to the owners manual of your model for the exact location and application of this part.NOTE: We do offer an article on ...