Line Striping & Marking Machines
Striping & Marking Machines

| Compare | Image | Capacity | Paint Type | Brand | Model # | Price | |
|---|---|---|---|---|---|---|---|
![]() | 20 oz. Aerosol Spray Cans (12 Spare Cans) | - | Global Industrial | Ships Same Day WB670691 | $139.95 | ||
![]() | 5 Gallon Pail | Latex/Oil Based | Newstripe | WBB1246619 | $3,999.00 | ||
![]() | 5 Gallon Pail | Water/Oil Based | Newstripe | WBB954907 | $2,999.00 | ||
![]() | 5 Gallon Pail | Water/Oil Based | Newstripe | Ships Same Day WBB284335 | $1,849.00 | ||
![]() | 1 Gallon Paint Can | Water/Oil Based | Newstripe | Ships Same Day WB239823 | $969.00 | ||
![]() | 20 oz. Aerosol Spray Cans (12 Spare Cans) | - | Aervoe | Ships Same Day WB442647 | $175.95 | ||
![]() | 5 Gallon Pail | Latex/Oil Based | Newstripe | WBB1246620 | See price in cart | ||
![]() | 20 oz. Aerosol Spray Cans (12 Spare Cans) | - | Rust-Oleum | Ships Same Day WBB686339 | $235.95 | ||
![]() | 20 oz. Aerosol Spray Cans (12 Spare Cans) | Water Based | Aervoe | Ships Same Day WB436734 | $189.95 | ||
![]() | 20 oz. Aerosol Spray Can | - | Rust-Oleum | WBB686497 | $399.95 |
Accessories for Striping & Marking Machines

Related Products
Sturdy, lightweight construction. Create 3-6" straight lines quickly and easily. Cover a larger area in a shorter time. Convenient storage compartment holds 12 extra cans. Sturdy steel construction. Collapsible handle for easy storage. Large diameter wheels to accommodate high grass conditions.
Solvent-based inverted striping paint for durable and bright long-lasting lines. Creates 800 linear feet (2" stripe); 400 linear feet (4" stripe). Highest solids for complete coverage. Dries fast less than 10 minutes. Guaranteed not to clog. Use with Striping Machine or Striping Wand (sold separately).
Rust-Oleum 2300 System Inverted Striping Paint Aerosol Red Solvent-based inverted striping paint for durable and bright long-lasting lines. Creates 800 linear feet (2" stripe); 400 linear feet (4" stripe). Highest solids for complete coverage. Dries fast less than 10 minutes. Guaranteed not to clog. Use with Striping Machine or Striping Wand (sold separately)
Rust-Oleum M1600 System Solvent-Based Precision-Line Inverted Marking Paint Aerosol Fluorescent Red Water and solvent-based marking paints feature a precision-line spray tip for easy-to-read bright, vivid markings for utility, construction, excavation, surveying, landscape, and golf course markings. Best resistance against premature fading. Marks more linear feet per can than other brands. No mess spray tip keeps paint off fingers. Locking tip does not pop off. Virtually no overspray. Dries fast less than 5 minutes. Convenient spray-through cap. Guaranteed not to clog
Newstripe's Rear Caster allows you to create the perfect circles and arcs. The Rear Caster quickly and easily lowers when needed to paint circles and arcs, then locks in the upright position for painting straight lines.
Related Items
inverted striping paint aerosolnewstripe 5 gallon fast dry paintnewstripe replacement hoselightweight line striper with wheelsRelated Categories
rust-oleum aerosol paintsLine Striping & Marking Machines for Parking Lots, Warehouses & Facilities
Line striping and marking machines apply straight, consistent painted lines to pavement, concrete, floors, grass, and other compatible surfaces. They are used to mark parking spaces, traffic lanes, pedestrian walkways, warehouse aisles, work zones, athletic fields, and other areas where clear visual boundaries are needed.
Striping machines range from simple aerosol applicators for smaller marking jobs to roller and airless systems designed for larger or more frequent projects. Choosing the right machine depends on the surface, size of the area, type of marking, paint requirements, and how often the equipment will be used.
What to Consider When Choosing a Line Striping Machine
Match the machine to the size and frequency of the striping work. A facility making occasional touch-ups has different equipment needs than a crew regularly striping large parking lots.
- Project size: Aerosol stripers can be practical for smaller jobs and touch-ups, while higher-capacity machines reduce interruptions on larger projects.
- Application method: Depending on the model, striping machines may apply paint from aerosol cans, paint containers, rollers, or pressurized airless systems.
- Surface: Check that the machine and selected paint are appropriate for asphalt, concrete, indoor floors, grass, dirt, or another intended surface.
- Paint compatibility: Machines vary in the types and containers of paint they accept. Review individual specifications before selecting paint.
- Line requirements: Consider the desired line width and whether adjustments are needed for parking spaces, aisles, traffic lanes, or other markings.
- Frequency of use: Occasional maintenance, routine facility striping, and high-volume commercial work can require different machine capacities and features.
- Portability and operation: Machine size, weight, maneuverability, and storage requirements can affect which model is practical for a facility or work crew.
Types of Line Striping & Marking Machines
The primary difference between striping machines is how they hold and apply paint. Understanding these differences can help narrow the choice based on project size and frequency of use.
| Type | How It Works | Best Suited For | What to Consider |
|---|---|---|---|
| Aerosol Line Stripers | Hold an aerosol marking paint can and apply paint as the machine is pushed | Touch-ups, smaller parking areas, facility markings, occasional use | Paint-can compatibility, line width, portability |
| Roller Striping Machines | Apply liquid paint with a roller as the machine moves | Parking lots, warehouses, indoor areas, routine line marking | Paint capacity, line width, surface, paint compatibility |
| Airless Line Stripers | Pump paint under pressure through a spray tip | Larger parking lots, roads, facilities, frequent striping projects | Capacity, pressure, output, paint compatibility, maintenance |
| Self-Propelled Stripers | Use powered movement to assist the operator while applying paint | Larger areas and higher-volume striping work | Project size, maneuverability, capacity, storage |
| Turf & Dirt Stripers | Apply marking paint to grass, soil, and similar outdoor surfaces | Athletic fields, landscaping, events, outdoor layouts | Surface and marking-paint compatibility |
Aerosol vs. Airless Line Striping Machines
Aerosol and airless striping machines can both produce painted lines, but they are suited to different levels of work.
Aerosol striping machines use replaceable cans of marking paint and typically require less setup. They can be practical for smaller areas, periodic maintenance, touch-ups, and facilities that do not perform large striping projects regularly.
Airless line stripers draw paint from a larger container and pump it through a spray tip under pressure. Their greater paint capacity makes them better suited to larger areas and frequent striping work where repeatedly changing aerosol cans would interrupt the job.
When comparing the two, consider project size, frequency of use, required capacity, paint compatibility, maintenance, and storage.
Common Uses for Striping & Marking Machines
Striping equipment can create visual boundaries and traffic patterns across commercial, industrial, institutional, and outdoor environments.
- Parking lots and garages: Mark parking spaces, traffic lanes, boundaries, and other pavement markings.
- Warehouses and distribution centers: Define aisles, work areas, equipment zones, storage areas, and designated pedestrian routes.
- Pedestrian walkways: Create visible pathways to help distinguish pedestrian travel areas from surrounding vehicle or equipment traffic.
- Manufacturing and industrial facilities: Mark traffic routes, staging areas, work zones, and other designated floor areas.
- Roads and private drives: Apply traffic markings where the machine, paint, layout, and application are appropriate for the project.
- Construction, jobsite, and maintenance areas: Establish temporary or permanent markings for traffic flow, work areas, and site organization.
- Athletic fields and grounds: Turf-compatible machines can mark playing fields, event layouts, and other outdoor areas.
How to Mark Pedestrian Walkways in Facilities
Clearly marked pedestrian walkways can help distinguish foot traffic from areas used by forklifts, vehicles, and other mobile equipment.
Before striping a walkway, determine the route and identify intersections, doorways, equipment areas, vehicle paths, and other points where pedestrian and vehicle traffic may interact. Prepare the surface according to the paint manufacturer's instructions, lay out the route, and use a compatible striping machine and paint to create visible, consistent markings.
Walkway width, color, placement, and other requirements can vary by facility and application. Review applicable safety requirements and site-specific conditions when establishing pedestrian routes rather than relying on paint color or line width alone.
Striping Machine Accessories & Maintenance
The right accessories can help maintain line quality and keep striping equipment operating properly. Depending on the machine, available accessories can include spray tips and nozzles, hoses, paint cups, lids, stands, and power conversion components.
Before ordering replacement parts or accessories, verify compatibility with the specific striping machine model. After use, follow the manufacturer's cleaning and maintenance instructions, particularly for components that come into contact with paint. Proper cleaning can help prevent dried paint from affecting spray patterns, rollers, tips, and other application components.
Frequently Asked Questions
Have a Question? Our experts might already have the answers.
What is a line striping machine used for?
A line striping machine applies painted lines and markings to compatible surfaces. Common uses include parking spaces, traffic lanes, warehouse aisles, pedestrian walkways, work zones, athletic fields, and other areas that require visible boundaries or traffic patterns.
What type of line striping machine should I choose?
Choose based on project size, surface, paint requirements, frequency of use, and desired capacity. Aerosol machines can be practical for smaller jobs and touch-ups, while roller, airless, and self-propelled machines may be better suited to larger or more frequent striping projects.
What is the difference between an aerosol and an airless line striper?
Aerosol stripers apply paint from replaceable spray cans and are useful for smaller or occasional projects. Airless stripers pump paint from a larger container through a spray tip under pressure, making them better suited to larger areas and frequent striping work.
Can line striping machines be used for parking lots?
Yes. Line striping machines are commonly used to mark parking spaces, traffic lanes, boundaries, and other pavement markings in parking lots and garages. Choose equipment and paint that are appropriate for the surface and project size.
Can striping machines be used in warehouses?
Yes. Striping machines can mark warehouse aisles, pedestrian routes, work areas, storage zones, and equipment traffic paths. Select paint and equipment that are compatible with the floor surface and facility requirements.
How do you mark pedestrian walkways in a warehouse or facility?
Plan the pedestrian route around vehicle paths, intersections, doorways, and work areas, then prepare the surface and apply visible, consistent markings using compatible paint and striping equipment. Walkway dimensions, colors, and placement should follow applicable requirements and site conditions.
Can the same striping machine be used on asphalt and concrete?
Some striping machines can be used on both asphalt and concrete, but suitability also depends on the paint and individual machine specifications. Check surface and paint compatibility before beginning the project.
Can line striping machines be used on grass?
Some striping and marking machines are specifically designed to apply marking paint to grass, dirt, and similar outdoor surfaces. Check that both the machine and marking paint are intended for turf or ground applications.
What paint should I use in a line striping machine?
Use paint that is compatible with the specific machine and intended surface. Striping machines may accept aerosol cans, water-based paint, oil-based paint, latex paint, or other formulations depending on the model. Always check the manufacturer's specifications.
How do you maintain a line striping machine?
Follow the manufacturer's cleaning and maintenance instructions after use. Paint-contact components such as spray tips, nozzles, hoses, rollers, and paint containers may require cleaning to help prevent dried material from affecting future operation.