Take 15% off your entire order!

Offer applied at checkout

NoTrax® Stages Entry Mat System

NoTrax® Stages Entry Mat System

NoTrax® Stages Entry Mat SystemPrelude™ is a scraper mat made up of a coarse loop-twisted non-absorbent fiber that can be placed outside the entrance to begin the removal of dirt and debris from foot traffic. These aggressive fibers resist crushing while entrapping debris and preventing it from entering the facility. This mat can be used as part of the coordinated "Stages" entrance matting system. A heavyweight vinyl non-slip backing ensures minimum movement.
Encore™ is an entrance mat that uses a combination of scraping and looped pile Decalon® drying yarns in a linear pattern, to facilitate the scraping function and begin the drying process. It can be used as a stand-alone mat, or as part of the "Stages" coordinated entrance matting system.
Ovation™ is made with a generously tufted Decalon® looped pile construction that serves as the finishing, drying and cleaning mat in the coordinated "Stages" entrance matting system, A heavyweight vinyl non-slip backing ensures minimum movement.