Aluminum Rollator with 6" Casters, Fold Up and Removable Back Support, Padded Seat, Blue

Rollover image to zoom in

Click image to enlarge

See all 41 items in product family

Aluminum Rollator with 6" Casters, Fold Up and Removable Back Support, Padded Seat, Blue

Item #: WBB275173

Sold By: globalindustrial.com

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $194.97 Save up to 63%
Qty Price
1 $77.95 ea.
2+ $71.95 ea.
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Aluminum Rollator with 6" Casters, Fold Up and Removable Back Support, Padded Seat, Blue

The Walker Rollator with 6" Wheels, Fold Up Removable Back Support and Padded Seat in Blue by Drive Medical comes standard with 6" caster wheels, loop locks and serrated brakes to ensure safety. The seamless padded seat opens to a roomy, convenient, zippered storage pouch to easily and securely transport personal items, and the ergonomic handles are easy to grip, relieve hand pressure, and are height adjustable to accommodate users height. This Rollator by Drive Medical is a great value that provides the freedom of mobility. With a convenient seat for resting and loop locks that keep the Rollator from moving, you can be assured that this mobility aid will provide a safe and secure way to regain your active lifestyle.

Features and Benefits:
  • Comes with new seamless padded seat
  • Zippered pouch under seat for added privacy and security of personal items
  • Removable, hinged, padded backrest can be folded up or down
  • 6" Black non-marring casters with soft grip tires are ideal for indoor and outdoor use
  • Easy-to-use deluxe loop locks
  • Loop locks on the handle can be pressed in the down position to lock the wheels and prevent movement
  • Brakes with serrated edges provide firm hold
Product Specifications:
  • Dimensions : 27.5"L x 24.5"W x 32"H
  • Handle Height : 32" - 37"
  • Color : Blue
  • Material : Aluminum
  • Weight Capacity : 300 lbs
  • Seat Depth : 12"
  • Seat Width : 14"
  • Seat to Floor Height : 20"
  • Seat to Foot Deck : 15.5" -18.5"
  • Warranty : Limited Lifetime
  • Assembly : Basic Assembly Required
Documents

Documents are in PDF format

Product Specifications

    • BRANDDrive Medical
    • MANUFACTURERS PART NUMBERR726BL
    • LENGTH27-1/2"
    • WIDTH24-1/2"
    • HEIGHT32" - 37"
    • WEIGHT LBS.12
    • WEIGHT CAPACITY300 lbs
    • DESCRIPTIONAluminum Rollator with 6" Casters
    • COLORBlue
    • SEAT WIDTH14"
    • SEAT DEPTH12"
    • SEAT HEIGHT20"
    • HANDLE HEIGHT32" - 37"
    • LIMITED WARRANTYLimited Lifetime
    • CASTERS6" Casters
    • SIZEAdult
    • PACKAGE QUANTITY1
    • TYPERollator

Avg. Customer Rating: (9 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Aluminum Walker

Just recieved these items yesterday. Fotna better price on each as i ordered 2 at the same time. They got lost in delivery and Global jumped right on it ans sent me 2 new ones. Easy to assemble...it was already mostly done. I have yet to have my aunt take one for a test run.

See more favorable reviews

The most critical review

  • Customer Rating
Sort by: 
1 ...

9 Results

Aluminum Walker

Your review: Just recieved these items yesterday. Fotna better price on each as i ordered 2 at the same time. They got lost in delivery and Global jumped right on it ans sent me 2 new ones. Easy to assemble...it was already mostly done. I have yet to have my aunt take one for a test run.

Is this review helpful?

Top of the Line

Your review: A walker advertised all over for around $200 on sale by Global for $70 and exactly the same as any top of the line walker. Global contacts very nice and easy to work with.

Pros: Never thought I'd rave about a walker--fought against using one for many months. But I am now a convert. This is so easy to use, to fold up, and to lift into my car.

Cons: 1) Not in stock--long wait for delivery. 2) No relationship with my health ins. company sso had to order this directly. (Really not a major problem considering thee price). 3) had to put it together myself or hire someone else to do it.

Is this review helpful?

Drive, Aluminum Fold Up Walker

Your review: I have used this for two months and find it an excellent walker. I would recommend this unit to anyone.

Pros: The light weight makes it easy to lift and very portable. Very easy to assemble. Great unit.

Cons: Cannot think of one.

Is this review helpful?

A GODsend

Your review: I recently had open-heart surgery and am still weak and a bit wobbly on my feet. The one time a year where I can see my sisters is at a Cranberry Festival. I bought the Rollator so I could attend the festival, while being able to get around. I did have to use the seat often, but I was able to spend hours with my sisters.

Pros: The seat is the reason I bought the Rollator, knowing that it was designed for big people (up to 300 pounds). I used it in my daily walks and it works well.

Cons: I read one review that said that the handle height was excellent for a person 6'1"--it was too low for me at 6".

Is this review helpful?

Increased mobility

Your review: Great product that provides increased mobility and a seat when needed

Pros: increased mobility, stability, seat, storage, folds up

Cons: none found

Is this review helpful?

what title

Your review: excellent walker

Pros: all good

Cons: none so far

Is this review helpful?

94-year old mother

Your review: Bought this for my mother. Husband and I love it. Mom won't use it. The brakes don't seem to work well on a large 8x10 rag rug in her den. I am wondering if different wheels would help?

Pros: I like everything about it.

Cons: Brakes may be a difficult for a 94 year old to grasp - no strength in her hands possible.

Is this review helpful?

Rollator

Your review: works great, very light weight. wish it were more adjustable

Pros: light weight

Cons: does not adjust height

Is this review helpful?

Perfect for me.

Your review: This rollator is the perfect width to go through my doors easily, is high enough for me to sit easily, and is lightweight enough for me to pick up with one hand! Love it.

Pros: Goes through home doors easily. Lightweight enough to pick up with one hand. Seat is high enough to sit down easily.

Cons: Brakes are a bit stiff to lock in place.

Is this review helpful?

Sort by: 
1 ...

9 Results

Be the First to Ask a Question!